Advanced Topics on the BQ40z80 - Current Scaling
Description
September 20, 2018
The BQ40z80 natively supports pack capacities up to 29Ah and battery currents up to 32A, and the BQ40z80 also includes a scale factor that can be set between 0 and 100 to “scale up” the currents seen by the coulomb counter. This video gives an overview of this function.
Additional information
This course is also a part of the following series
Date: July 29, 2019
Date: October 8, 2018