Email

Advanced Topics on the BQ40z80 - Current Scaling

Description

September 20, 2018
The BQ40z80 natively supports pack capacities up to 29Ah and battery currents up to 32A, and the BQ40z80 also includes a scale factor that can be set between 0 and 100 to “scale up” the currents seen by the coulomb counter. This video gives an overview of this function.

Additional information

This course is also a part of the following series

Date: October 8, 2018
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki