AM57x Sitara™ processors

Email

How to Use AM57x/DRA7x DFU Boot Mode with Linux Host

Description

July 11, 2017

This video demonstrates how to use the DFU (Device Firmware Upgrade) boot mode on AM57x and DRA7x processors, both of which support peripheral booting from a USB host. It provides setup information for both the Linux host and the device to be booted (in this example, a Jacinto 6 EVM) , walks through the DFU command flow and compiling of the u-boot image, and then demonstrates the full DFU boot sequence from the perspective of both the EVM and the host.

Download webinar slides

Additional information

arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki