8.1 Closed-loop Delfino control systems: Implementating multiprotocol communications with AMIC109
Description
April 17, 2017
This training presents the AMIC110 architecture and shows how it interfaces with the Delfino MCU. It also provides an overview of TIDA-00299, which is the TI Design that demonstrates multiprotocol industrial communications using the AMIC110 ICE Board in combination with the C2000 Delfino LaunchPad.
Download webinar slides
Additional information
This course is also a part of the following series
Date: April 17, 2017