C2000™ MCU device workshops

Email

C2000™ LF240x Microcontroller Workshop

Description

May 15, 2019

NOTE: The workshop materials on this page are no longer being updated or maintained, and are provided “as is”. However, the workshop materials can still be very useful for learning about the device. The CCS projects which are used with the lab exercise source files may need to be recreated for use with later versions of the software. Also, the hardware target (i.e. development board) may be discontinued.

The C2000 TMS320LF240x Microcontroller Workshop is a hands-on technical course based on the TMS320LF2407A device. Learning is accomplished through detailed presentation materials and hands-on lab exercises. This workshop has been developed to decrease the learning curve from months to days, reduce development time, and accelerate product time to market. Also, this workshop is perfect for both the beginner and advanced users.

The workshop starts with the basic concepts and progresses to more advanced topics in a logical fashion. Each topic and lab exercise builds on the previous one that was presented, running a common theme throughout the workshop. All of the lab exercises are written in assembly and are performed on the Spectrum Digital EVM320LF2407A Evaluation Module. The materials guide the user through system initialization, peripheral setup, and programming an application into flash memory.

Workshop Outline

  1. Introduction and Architectural Overview
  2. Program Development Tools
  3. Addressing Modes
  4. Basic Programming Techniques
  5. Advanced Programming Techniques
  6. Numerical Issues
  7. Implementing Algorithms
  8. Logical Operations
  9. System Initialization
  10. Interrupts
  11. Analog-to-Digital Converter
  12. Event Manager
  13. System Design
  14. Communications
  15. C Compiler
  16. Development Support

Running the Labs

In order to run the labs, you will need:

Workshop Materials - Revision 4.2 February 2002

Additional information

This course is also a part of the following series

arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki