Connect: Software Robustness
Description
August 22, 2018
Henry Wiechman, a TI software expert will walk through the full SimpleLink™ software development process, including testing, release cadence, interoperability, and more. The SimpleLink software development kit offers 100% code portability from one SimpleLink platform device to another so the team won’t have to start over with new code or make massive changes to the code base. Team members also won’t have to learn new tools to use the small amount of new application code needed for new features. |
Additional information
This course is also a part of the following series
Date: July 10, 2018
Date: April 3, 2019