3.5 Connect: Vibration Condition Monitoring Demo
Description
In this episode, Amit will showcase an example of predictive maintenance, called vibration condition monitoring, using the SimpleLink MSP432p4111 MCU and the CC26x2 Bluetooth low energy wireless MCU (SoC). The ability to predict the life of a motor gives an operator the ability to optimize maintenance schedules of often costly and large motors/pumps while improving the operational lifetime of the production lines using these motors, often without any lapse in production.