Email

2.13 Connect: Wi-Fi 5-GHz

Watch the next video in the series:

Details

Date: February 22, 2019

This week on Connect, Andrew, a SimpleLink product marketing engineer, answers some commonly asked questions from the Connect community around the new dual-band (2.4 GHz + 5-GHz)  SimpleLink Wi-Fi wireless MCUs and how you can get better performance while maintaining excellent power consumption with 5-GHz.  

The dual-band CC3235x device comes in two variants, CC3235S and C3235SF:

  • The CC3235S includes 256KB of RAM, IoT networking security, device identity/keys, as well as, MCU level security features such as file system encryption, user IP (MCU image) encryption, secure boot and debug security.
  • The CC3235SF builds on the CC3235S and integrates a user-dedicated 1MB of executable flash in addition to the 256KB of RAM.

These devices are also offered as fully programmable FCC, ISED/IC, ETSI/CE, and MIC CERTIFIED wireless microcontroller modules.

arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki