Email

Creating IoT Solutions with TM4C Microcontrollers Workshop Series 15 of 16: Low Power Modes

with Scott Bland

Details

Date: February 20, 2015

This chapter covers Low Power Modes from the Creating IoT Solutions with TM4C Microcontrollers.

 

Additional information

Preface

The intent of this workshop is to be a place where a person with a few C skills and some microcontroller experience can familiarize themself with the Tiva TM4C129x series parts, Code Composer Studio, TivaWare for C Series and the process of programming these microcontrollers. If you lack C programming skills, there are many courses on the Internet where you can gain them ... that knowledge can form the basis for a rewarding career.

If you are migrating from earlier Stellaris devices, please refer to this documnt for more information.

Overview

The Creating IoT Solutions with the Tiva C Series Connected LaunchPad Workshop is an in-depth, hands-on introduction into the basics of creating IoT solutions using the EK-TM4C1294XL Connected LaunchPad including:

Connected LaunchPad Board
  1. Intro to TM4C Devices, LaunchPad and Cloud Services
  2. Intro to Code Composer Studio
  3. TivaWare, Initialization and GPIO
  4. Ethernet Port
  5. Interrupts and the Timers
  6. ADC and the Educational Boosterpack
  7. PWM and QEI
  8. I2C, SensorLib and GUI Composer
  9. SPI and the QSSI
  10. UART
  11. USB
  12. Memory, Security and the MPU
  13. Floating Point Unit
  14. DMA
  15. Low Power Modes
  16. Graphics Library

Each chapter includes an in-depth lab that will step you through the usage, programming and testing of the peripheral(s) or tool(s) covered.

Details

The workshop is based on the low cost, expandable EK-TM4C1294XL Connected LaunchPad Evaluation Kit. The LaunchPad board features a 120MHz TM4C1294NCPDT microcontroller, on-board emulation and 2 sets of 40-pin BoosterPack XL format expansion pins. The TM4C1294NCPDT microcontroller has 1MB of flash memory, 256kB of RAM, 6KB of EEPROM, two 12-bit 2MSPS analog to digital converters, a USB 2.0 OTG/H/D port, an Ethernet port, a hibernation module, motion control, other serial connectivity and flexible GPIO.

TI's Tiva C Series (TM4C129x) devices are supported by several Integrated Development Environments:

The workshop labs are based on Code Composer Studio, which is free and fully functional when connected to the Connected LaunchPad board.

The workshop labs are constructed using TivaWare™. TivaWare is an extensive suite of license and royalty-free software designed to simplify and speed development of Tiva C Series (TM4C129x) based microcontroller applications. TivaWare includes:

  • the Peripheral Driver Library which is a set of functions for controlling the peripherals found on the Tiva C Series (TM4C129x) family of ARM Cortex-M microcontrollers. This library comes preprogrammed in the ROM memory of all TM4C devices.
  • the TivaWare Graphics Library which is a set of graphics primitives and widgets for creating graphical user interfaces on TIVA C Series (TM4C129x) microcontroller-based boards that have a graphical display.
  • The Sensor Library which includes an I2C master driver, APIs for easily communicating over the I2C bus and examples for using the sensors on the SensorHub BoosterPack.

 

Expandability of the LaunchPad board is accomplished through its BoosterPack XL connectors. These connectors are backwards compatible with the original BoosterPack connectors. There are many BoosterPacks available through TI and third parties.

Hardware Requirements

To run the labs, you will need the following:

Software Requirements

To run the labs, you will need the following:

Complete instructions for downloading and installing this software can be found in Chapter 1 of the workbook

 

Workshop Material