Email

Pass CISPR 25 Class 5 without metallic shielding or common-mode choke

Description

September 11, 2017

EMI mitigation is commonly one of the most challenging aspects of a power supply design. This challenge is amplified in the automotive world, where meeting stringent CISPR 25 Class 5 standards are often mandatory. The LMS3635-Q1 and LMS3655-Q1 synchronous buck converters aid in the process of optimizing for EMI in several ways:

1) By eliminating wire-bonding in the package, parasitics that cause high-frequency switch-node ringing are also eliminated

2) A symmetrical and thoughtful pin-out enables the minimization of the size of the current loops

3) Spread spectrum lowers the peak radiated and conducted emissions

Watch as Katelyn uses the TIDA-01388 dual USB reference design to demonstrate how these devices pass CISPR 25 Class 5 without the use of metallic shielding or a common-mode choke. 

Additional information

This course is also a part of the following series

arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki