The End-of-Service Determination Algorithm
Description
September 30, 2018
The End-of-Service determination module provides information on the degradation of a battery used in a rarely discharged system, such as a backup battery or UPS. The device requires only a small ~1-2% discharge to evaluate the battery, thereby preserving 98+% of the battery capacity for use in a backup event.
Additional information
This course is also a part of the following series
Date: July 29, 2019
Date: October 8, 2018