Email

Extend speaker battery life: Smart amp class H efficiency

Description

January 10, 2019
The demo will showcase two identical speakers, one using older analog boosted class-d amp and the other using newest Smart amp with class H boost. Both EVM setups will be connected to a power monitor which will show energy consumption in real-time. The input voltage can be manually changed to emulate a battery discharging and visitors can see the energy savings are best when the battery is low.

Additional information

arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki