1.5 Hercules How to Tutorial: Force a Clock Monitor Failure
Description
March 10, 2015
This video highlights the clock monitoring circuitry integrated into many Hercules Safety MCUs. It provides an overview of the module and shows how to create initialization code for the Error Signaling Module (ESM) and the clock monitor using HALCoGen. Code Composer Studio is then used to create and deploy a project using the ESM and clock monitor on a Hercules USB Development Stick Kit that can be used to show the behavior of the MCU when the signal from the external crystal is disrupted. |
.