Email

5.1 How to design 1-phase shunt electricity meters using standalone metrology ADCs: Current detection mode overview

Details

Date: March 27, 2019
This module provides an overview of the ADS131M04’s current detection mode, which is a special low-power mode of the ADS131M04 standalone ADC that can detect the presence of current when someone has tampered with a meter by removing its neutral connection.  This is the first of two modules for the “ADS131M04 current detection mode for detecting neutral removal tampering” section of the “How to design 1-phase shunt electricity meters using standalone metrology ADCs” training series.
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki