How to Use AM57x/DRA7x DFU Boot Mode with Linux Host
説明
2017年 7月 11日
This video demonstrates how to use the DFU (Device Firmware Upgrade) boot mode on AM57x and DRA7x processors, both of which support peripheral booting from a USB host. It provides setup information for both the Linux host and the device to be booted (in this example, a Jacinto 6 EVM) , walks through the DFU command flow and compiling of the u-boot image, and then demonstrates the full DFU boot sequence from the perspective of both the EVM and the host.