Anti-tamper techniques to thwart attacks on smart meters

メール

4.2 Hardening a meter against magnetic tamper attacks: Transformer based high-side power supplies

説明

2017年 4月 12日

In order to use the AMC1304 for isolated shunt sensing, it is necessary to provide power to the high-side power supply of the AMC1304.  One option for this high-side power supply is to derive this power from the controller side power supply of the AMC1304 using a combination of a transformer driver such as the SN6501, a transformer, and rectification circuitry.  This module covers the advantages and disadvantages of using this transformer-based power supply to power the high-side of the AMC1304.  In addition, details will be provided on the TIDA-00601 and TIDA-01088 reference designs, which use a high-side transformer-based power supply.

This is the second of three modules for the “Hardening a meter against magnetic tamper attacks” section of the “Anti-tamper Techniques to Thwart Attacks on Smart Meters” training series.  

追加情報

arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki