C2000™ MCUs - Workshops

メール

1.1 C2000™ F28004x Microcontroller Workshop

説明

2019年 5月 14日

NOTE: This workshop is applicable to the TMS320F28002x device family.

The C2000 TMS320F28004x Microcontroller Workshop is a hands-on technical course based on the TMS320F280049C device. This device shares many common features and peripherals that are also found on the other C2000 family members. Therefore, this workshop is ideal for anyone interested in learning more about the C2000 microcontrollers. Learning is accomplished through detailed presentation materials and hands-on lab exercises. This workshop has been developed to decrease the learning curve from months to days, reduce development time, and accelerate product time to market. Also, this workshop is perfect for both the beginner and advanced users.

The workshop starts with the basic concepts and progresses to more advanced topics in a logical fashion. Each topic and lab exercise builds on the previous one that was presented, running a common theme throughout the workshop. All of the lab exercises are written using the Peripheral Driver Library and are performed on the F280049C LaunchPad development kit. The materials guide the user through system initialization, peripheral setup, and programming an application into flash memory using the Code Composer Studio on-chip flash programmer.

Workshop Outline

  1. Architecture Overview
  2. Programming Development Environment -- Lab: Linker command file
  3. Peripheral Register Programming
  4. Reset and Interrupts
  5. System Initialization -- Lab: Watchdog and interrupts
  6. Analog Subsystem -- Lab: Build a data acquisition system
  7. Control Peripherals -- Lab: Generate and graph a PWM waveform
  8. Direct Memory Access (DMA) -- Lab: Use DMA to buffer ADC results
  9. Control Law Accelerator (CLA) -- Lab: Use CLA to filter PWM waveform
  10. System Design -- Lab: Run the code from flash memory
  11. Communications -- Lab: SCI echoback from C2000Ware
  12. Support Resources

Running the Labs

In order to run the labs, you will need:

NOTE: Your CCS installation must include the following options in each category:
• Processor Support – select “C2000 real-time MCUs”
• Select Emulators – choose “TI XDS Debug Probe Support”

Workshop Materials - Revision 1.0 July 2019

追加情報

このコースは、次のシリーズに属します

Date: 5月16日2019年
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki