Connect: SimpleLink™ マイコン

メール

1.7 Connect: What is a sensor controller?

説明

2018年 11月 21日

The Sensor Controller is a small programmable CPU core that is highly optimized for low power consumption and efficient peripheral operation. It can perform simple background tasks autonomously and allow the System CPU and MCU to remain in sleep mode. This allows for power optimization based on events such as wake on temperature, wake on touch, and beyond.  It is fully configurable by the developer who can write and download code through the free online sensor controller studio.

追加情報

このコースは、次のシリーズに属します

Date: 7月10日2018年
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki