2.13 Connect: Wi-Fi 5-GHz
説明
2019年 2月 22日
This week on Connect, Andrew, a SimpleLink product marketing engineer, answers some commonly asked questions from the Connect community around the new dual-band (2.4 GHz + 5-GHz) SimpleLink Wi-Fi wireless MCUs and how you can get better performance while maintaining excellent power consumption with 5-GHz.
The dual-band CC3235x device comes in two variants, CC3235S and C3235SF:
- The CC3235S includes 256KB of RAM, IoT networking security, device identity/keys, as well as, MCU level security features such as file system encryption, user IP (MCU image) encryption, secure boot and debug security.
- The CC3235SF builds on the CC3235S and integrates a user-dedicated 1MB of executable flash in addition to the 256KB of RAM.
These devices are also offered as fully programmable FCC, ISED/IC, ETSI/CE, and MIC CERTIFIED wireless microcontroller modules.
追加情報
Tweet Nick @sensortocloud with future topic ideas!