メール

MCT8316ZTEVM getting started video

説明

2021年 7月 9日

This video shows how to spin a 3-phase BLDC motor in less than 10 minutes using the MCT8316ZTEVM Evaluation Module and MCT8316ZTEVM GUI. The video demonstrates how to connect a 3-phase motor, power supply, and hall sensors to the MCT8316ZTEVM. After powering the board, you can use the onboard potentiometer to control the speed of the motor which spins with a simple sensored trapezoidal algorithm. An MSP430FR2355 MCU and FTDI chip provides a connection to the MCT8316ZTEVM GUI to calculate the speed of the motor from the frequency generator output signal. The MCT8316Z is a 4.5-V to 35-V, 8-A peak integrated three-phase gate driver IC with sensored trapezoidal control for motor drive applications. It provides three integrated half-bridges and a sensored trapezoidal algorithm capable of directly driving a 3-phase brushless-DC motor. The hardware interface variant (MCT8316ZT) integrates an adjustable buck regulator, protection features, and flexible parameter settings such as slew rate control and buck output voltage

追加情報

arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki