ヒント:複数の語句はコンマで区切ってください

入力例:11/27/2021

入力例:11/27/2021

ヒント:複数の語句はコンマで区切ってください

入力例:11/27/2021

入力例:11/27/2021

並べ替え:

61 結果
UCD3138 Digital Power Training Series

The UCD3138 Digital PWM (DPWM) Module: Solution to firmware task

日付:
2016年 2月 26日

所要時間::
00:29
The solution to the lab 2 firmware task. Part of the "The UCD3138 Digital PWM (DPWM) Module" series.  
UCD3138 Digital Power Training Series

The UCD3138 Digital PWM (DPWM) Module: Setting the PWM period

日付:
2016年 2月 26日

所要時間::
03:58
This video shows how to set the DPWM period with firmware.    
UCD3138 Digital Power Training Series

The UCD3138 Digital PWM (DPWM) Module: Memory debugger hyperknob demonstration

日付:
2016年 2月 26日

所要時間::
04:29
This tutorial introduces the UCD Device GUI memory debugger hyperknob, which allows modification of the DPWM output waveforms remotely via PMBus. Part of the "T
UCD3138 Digital Power Training Series

The UCD3138 Digital PWM (DPWM) Module: Introduction to the Digital PWM (DPWM) Module

日付:
2016年 2月 26日

所要時間::
03:59
This video introduces the three digital power peripherals, focusing on the DPWM module. 
UCD3138 Digital Power Training Series

The UCD3138 Digital PWM (DPWM) Module: Firmware overview and DPWM demonstration

日付:
2016年 2月 26日

所要時間::
04:06
This video presents lab 2 - firmware, and shows the DPWM output waveforms on an oscilloscope.  
UCD3138 Digital Power Training Series

The UCD3138 Digital PWM (DPWM) Module: Controlling the DPWM outputs

日付:
2016年 2月 26日

所要時間::
08:30
How to write firmware to create simple waveforms on the two DPWM outputs.  
UCD3138 Digital Power Training Series

The UCD3138 Digital Filter Module: Solution to firmware tasks

日付:
2016年 2月 26日

所要時間::
05:56
This video presents the solution to the lab 2 firmware.   
UCD3138 Digital Power Training Series

The UCD3138 Digital Filter Module: Overview of DPWM operation in normal mode

日付:
2016年 2月 26日

所要時間::
08:59
The previous tutorial  discussed DPWM operation in open loop mode, where the PWM output was determined solely by the values of the DPWM registers.This video sho
UCD3138 Digital Power Training Series

The UCD3138 Digital Filter Module: Overview of Digital Filter architecture and operation

日付:
2016年 2月 26日

所要時間::
12:57
The UCD3138 filter is a PID filter with many enhancements added specifically for power supply control. In this video we discuss it's architecture and operation.
UCD3138 Digital Power Training Series

The UCD3138 Digital Filter Module: Introduction to the Digital Filter Module

日付:
2016年 2月 26日

所要時間::
05:13
This training introduces the digital filter module, which is used as the compensator in the closed loop system provided by the UCD3138 family of devices. This m
UCD3138 Digital Power Training Series

The UCD3138 Digital Filter Module: Introducing the loop mux

日付:
2016年 2月 26日

所要時間::
03:44
This video introduces the Loop Mux. The loop mux controls the connections between the different parts of the control loop – the Front End, the Filter, and the D
UCD3138 Digital Power Training Series

The UCD3138 Digital Filter Module: Coding tasks for this tutorial

日付:
2016年 2月 26日

所要時間::
03:09
This video presents the coding tasks for this tutorial, which are related to initialization of the digital filter module.  
UCD3138 Digital Power Training Series

The UCD3138 Digital Filter Module: Avoiding shoot-through

日付:
2016年 2月 26日

所要時間::
03:22
If the rising edge of DPWMB exceeds event 4, it causes shootthrough - as both DPWMA and DPWMB are on at the same time. This could have catastrophic consequences
UCD3138 Digital Power Training Series

The UCD3138 Analog Front End (AFE) Module: Triggering the EADC

日付:
2016年 2月 29日

所要時間::
01:31
The EADC sample trigger comes from a DPWM module. This tutorial explains how to route a sample trigger from DPWM0 to Front End 0 via the loop mux. 
UCD3138 Digital Power Training Series

The UCD3138 Analog Front End (AFE) Module: The AFE reference DAC

日付:
2016年 2月 29日

所要時間::
01:08
The front end module's reference DAC is used as the reference against which the power supply sensed feedback signal is compared. This tutorial explains how to s
UCD3138 Digital Power Training Series

The UCD3138 Analog Front End (AFE) Module: Setting up the open loop board for the closed loop demo

日付:
2016年 2月 29日

所要時間::
04:11
This video shows how to setup the UCD3138 open loop board for the closed loop demonstration. This closed loop demo uses all three Digital Power Peripherals and
UCD3138 Digital Power Training Series

The UCD3138 Analog Front End (AFE) Module: Other AFE features

日付:
2016年 2月 29日

所要時間::
02:15
Other AFE features are touched upon in this video, such as averaging the EADC output, using the front end module as a lower bandwidth and higher accuracy Succes
UCD3138 Digital Power Training Series

The UCD3138 Analog Front End (AFE) Module: Introduction to the Analog Front End Module (AFE)

日付:
2016年 2月 29日

所要時間::
02:29
This video introduces the front end module and discusses its basic operation. 
UCD3138 Digital Power Training Series

The UCD3138 Analog Front End (AFE) Module: Firmware overview and closed loop demo

日付:
2016年 2月 29日

所要時間::
03:24
This video explains the firmware required to create the closed loop and shows key signals on the open loop board on an oscilloscope. 
UCD3138 Digital Power Training Series

The UCD3138 Analog Front End (AFE) Module: Error ADC (EADC) Overview

日付:
2016年 2月 29日

所要時間::
06:17
This video introduces the Error Analog to Digital Converter (EADC). The EADC is the heart of the front end module.   
61 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki