ヒント:複数の語句はコンマで区切ってください

入力例:12/04/2021

入力例:12/04/2021

ヒント:複数の語句はコンマで区切ってください

入力例:12/04/2021

入力例:12/04/2021

並べ替え:

78 結果
Example signal enable circuits.

Enable or Disable a Digital Signal

日付:
2017年 11月 16日

所要時間::
02:19
How to use logic to enable or disable a signal.

Low Voltage Translation using SN74AXC8T245

日付:
2018年 2月 21日

所要時間::
04:09
This video introduces the industry's low voltage translator, SN74AXC8T245 along with an application to demonstrate the translation using the SN74AXC8T245EVM
Slow or noisy inputs can cause erroneous outputs.

Eliminate Slow or Noisy Input Signals

日付:
2018年 3月 28日

所要時間::
02:02
How to eliminate slow or noisy input signals.
Some signals need to be held while the system controller is off.

Hold a Signal During Controller Reset

日付:
2018年 3月 28日

所要時間::
01:56
How to use logic to hold a signal line high or low while the system controller is powered off or held in reset.
Systems can have multiple error flags that need to be monitored.

Use Fewer Inputs to Monitor Error Signals

日付:
2018年 3月 28日

所要時間::
01:59
How to use logic gates to reduce the number of inputs required to monitor multiple error flags.

Standard Logic - CMOS Inputs

日付:
2018年 5月 3日

所要時間::
12:40
Introduction to the Standard Logic and Translation Family. Includes generic CMOS input structure and use cases

Understanding schmitt trigger

日付:
2018年 5月 3日

所要時間::
05:24
Understanding Schmitt trigger

CMOS Logic Outputs

日付:
2018年 5月 3日

所要時間::
07:21
Understanding CMOS outputs

Signal Level Translation

日付:
2018年 5月 3日

所要時間::
02:03
Level translation for standard Interfaces

Understanding Flip-flops,shift registers

日付:
2018年 5月 3日

所要時間::
05:07
Understanding Shift Registers and Flip-flops
2N7001T Unidirectional Level Shifter

Introducing the 2N7001T level shifter

日付:
2018年 5月 21日

所要時間::
04:59
This video introduces the 2N7001T a 1-bit unidirectional level shifter device that can be used in place of discrete push-pull level shifting implementations.
Pitfalls of Discrete Push-Pull Level Shifting

Understanding the pitfalls of discrete level shifting circuits

日付:
2018年 5月 21日

所要時間::
08:23
This video outlines common drawbacks to discrete push-pull level shifting implementations, introducing the 2N7001T device as a discrete replacement.

Discrete Level Translation Replacement

日付:
2018年 5月 23日

所要時間::
00:33
Watch this EVM for 2N70001T, which is a single channel unidirectional level translation intended for Replacement of discreet channel FET.
Automotive Current Shunt Monitoring

Automotive Current Monitoring Using High Speed Amplifiers

日付:
2018年 5月 24日

所要時間::
05:11
Automotive Current Monitoring Using High Speed Amplifiers

Logic and voltage translation

A list of all videos on training.ti.com related to logic and voltage translators that are not produced under the The Logic Minute.
Schematic representation of matching inverted clock inputs with an inverter.

Synchronize Inverted Clock Inputs

日付:
2018年 6月 29日

所要時間::
01:04
How to synchronize devices with inverted clock inputs operating off the same clock source.
Examples of systems that might need a power on reset signal.

Generate a Reset Signal at System Power On

日付:
2018年 6月 29日

所要時間::
01:13
How to generate a power on reset signal.
What a logic part is based on its part name. What a part name means

Anatomy of a logic part number

日付:
2018年 8月 22日

所要時間::
01:27
Logic part numbers use a formulaic naming system to denote the device's functionality and features. This video reviews the components to a logic part's name.
Understanding Bus Hold Functionality for Level Translators

Understanding Bus Hold Functionality for Level Translators

日付:
2018年 9月 8日

所要時間::
02:32
This video provides an overview of the bus hold functionality found on many level translators and its suitability for use within applications.
Schematic representation of a D-Type Flip-Flop to toggle a system on or off using a momentary switch.

Convert a Momentary Switch to a Toggle Switch

日付:
2018年 9月 11日

所要時間::
01:31
How to use logic to utilize a momentary switch in place of a toggle switch.
78 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki