ヒント:複数の語句はコンマで区切ってください

入力例:07/31/2021

入力例:07/31/2021

ヒント:複数の語句はコンマで区切ってください

入力例:07/31/2021

入力例:07/31/2021

並べ替え:

73 結果

Discrete Level Translation Replacement

日付:
2018年 5月 23日

所要時間::
00:33
Watch this EVM for 2N70001T, which is a single channel unidirectional level translation intended for Replacement of discreet channel FET.
Pitfalls of Discrete Push-Pull Level Shifting

Understanding the pitfalls of discrete level shifting circuits

日付:
2018年 5月 21日

所要時間::
08:23
This video outlines common drawbacks to discrete push-pull level shifting implementations, introducing the 2N7001T device as a discrete replacement.
2N7001T Unidirectional Level Shifter

Introducing the 2N7001T level shifter

日付:
2018年 5月 21日

所要時間::
04:59
This video introduces the 2N7001T a 1-bit unidirectional level shifter device that can be used in place of discrete push-pull level shifting implementations.

Signal Level Translation

日付:
2018年 5月 3日

所要時間::
02:03
Level translation for standard Interfaces

Understanding Flip-flops,shift registers

日付:
2018年 5月 3日

所要時間::
05:07
Understanding Shift Registers and Flip-flops

Understanding schmitt trigger

日付:
2018年 5月 3日

所要時間::
05:24
Understanding Schmitt trigger

CMOS Logic Outputs

日付:
2018年 5月 3日

所要時間::
07:21
Understanding CMOS outputs

Standard Logic - CMOS Inputs

日付:
2018年 5月 3日

所要時間::
12:40
Introduction to the Standard Logic and Translation Family. Includes generic CMOS input structure and use cases
Some signals need to be held while the system controller is off.

Hold a Signal During Controller Reset

日付:
2018年 3月 28日

所要時間::
01:56
How to use logic to hold a signal line high or low while the system controller is powered off or held in reset.
Systems can have multiple error flags that need to be monitored.

Use Fewer Inputs to Monitor Error Signals

日付:
2018年 3月 28日

所要時間::
01:59
How to use logic gates to reduce the number of inputs required to monitor multiple error flags.
Slow or noisy inputs can cause erroneous outputs.

Eliminate Slow or Noisy Input Signals

日付:
2018年 3月 28日

所要時間::
02:02
How to eliminate slow or noisy input signals.

Low Voltage Translation using SN74AXC8T245

日付:
2018年 2月 21日

所要時間::
04:09
This video introduces the industry's low voltage translator, SN74AXC8T245 along with an application to demonstrate the translation using the SN74AXC8T245EVM
Example signal enable circuits.

Enable or Disable a Digital Signal

日付:
2017年 11月 16日

所要時間::
02:19
How to use logic to enable or disable a signal.
Schematic representation of power good signal combination.

Combining Power Good Signals

日付:
2017年 11月 16日

所要時間::
02:20
How to overcome parasitic capacitance when using power good signals.

Introduction to the AXC family of direction controlled translation device

日付:
2017年 11月 7日

所要時間::
03:57
This video provides an introduction to the latest direction controlled translation device from TI- SN74AXC1T45.

The Logic Minute – Logic and translation

The Logic Minute video series makes complex ideas related to logic and translation easy to understand in just a couple of minutes.
Multi-voltage translation schematic for the LSF family of devices.

Multi-voltage Translation with the LSF Family

日付:
2017年 10月 17日

所要時間::
02:56
How to use a single LSF device to translate between multiple voltages in the same system.
Single supply translation schematic for the LSF family of devices.

Single Supply Translation with the LSF Family

日付:
2017年 10月 17日

所要時間::
02:12
How to use the LSF when there are supply limitations.
Internal schematic for up translation with an LSF family device.

Up Translation with the LSF Family

日付:
2017年 10月 17日

所要時間::
05:39
A deep look at how an LSF device achieves up translation.
Internal schematic for an LSF down translation circuit.

Down Translation with the LSF Family

日付:
2017年 10月 17日

所要時間::
03:18
A deep look at how an LSF device achieves down translation.
73 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki