ヒント:複数の語句はコンマで区切ってください

入力例:10/19/2019

入力例:10/19/2019

ヒント:複数の語句はコンマで区切ってください

入力例:10/19/2019

入力例:10/19/2019

並べ替え:

36 結果
What a logic part is based on its part name. What a part name means

Anatomy of a Logic Part Number

日付:
2018年 8月 22日

所要時間::
01:34
Logic part numbers use a formulaic naming system to denote the device's functionality and features. This video reviews the components to a logic part's name.

Application specifc logic videos

Logic's diverse portfolio touches every corner of the electronic industry; we are in a unique position to offer insight into a set of uses cases relevant to a particular group of systems and equipment.

Basics of Logic and Translation

In this section, the logic experts provide short lessons on standard logic devices ranging from basic applications up through a technical analysis of device operation. 

Choosing the right auto bidirectional voltage translator

日付:
2019年 7月 5日

所要時間::
02:36
How to decide which family of auto bidirectional voltage translators to use.

Common applications of Logic

Some design challenges are prevalent across many systems. In this section, these common challenges are overcome utilizing logic devices to aid in optimizing system design. These videos include an understanding of the problem being solved, and a description of one or more solutions to these issues.

Discrete Level Translation Replacement

日付:
2018年 5月 23日

所要時間::
00:33
Watch this EVM for 2N70001T, which is a single channel unidirectional level translation intended for Replacement of discreet channel FET.
Internal schematic for an LSF down translation circuit.

Down Translation with the LSF Family

日付:
2017年 10月 17日

所要時間::
03:19
A deep look at how an LSF device achieves down translation.
Slow or noisy inputs can cause erroneous outputs.

Eliminate Slow or Noisy Input Signals

日付:
2018年 3月 28日

所要時間::
02:02
How to eliminate slow or noisy input signals.

Enabling Image Sensor to Process Interfaces with Level Translation

日付:
2018年 12月 21日

所要時間::
04:15
Enabling IP camera image sensor to processor interfaces with voltage translation
2N7001T Unidirectional Level Shifter

Introducing the 2N7001T level shifter

日付:
2018年 5月 21日

所要時間::
04:59
This video introduces the 2N7001T a 1-bit unidirectional level shifter device that can be used in place of discrete push-pull level shifting implementations.
Introduction to the SN74AXC2T45 two channel voltage level translator

Introduction to the SN74AXC2T45 two channel low voltage direction controlled level translator

日付:
2019年 4月 30日

所要時間::
03:06
Introduction to the SN74AXC2T45 two channel low voltage direction controlled level translator
Introduction to the SN74AXC4T245 four bit voltage level translator

Introduction to the SN74AXC4T245 four bit low voltage direction controlled level translator

日付:
2018年 12月 21日

所要時間::
03:03
Key features and benefits of the SN74AXC4T245 four bit low voltage direction controlled level translator
sn74axc4t774

Introduction to the SN74AXC4T774

日付:
2019年 7月 5日

所要時間::
03:22
Learn about the key features and benefits of the SN74AXC4T774 four bit low voltage direction controlled level translator.
Introduction to the SN74AXCH4T245 four bit voltage level translator

Introduction to the SN74AXCH4T245 four bit low voltage direction controlled level translator with bus hold

日付:
2019年 4月 4日

所要時間::
03:49
Introduction to the SN74AXCH4T245 four bit low voltage direction controlled level translator
SN74AXCH8T245 an eight bit direction controlled level translator with bus hold functionality

Introduction to the SN74AXCH8T245 eight bit direction controlled level translator with bus hold functionality

日付:
2018年 9月 14日

所要時間::
04:00
This video provides an introduction to the latest direction controlled translation device from TI- SN74AXCH8T245.
Schematic representations for each LSF device in the family

Introduction – Voltage Level Translation with the LSF Family

日付:
2017年 10月 17日

所要時間::
01:25
Introduction to the LSF video series and the LSF family of devices

Logic and Voltage Translation Videos

A list of all videos on training.ti.com related to logic and voltage translators that are not produced under the The Logic Minute, the technical video series created by the experts on logic and voltage translation devices.

Multi-voltage translation schematic for the LSF family of devices.

Multi-voltage Translation with the LSF Family

日付:
2017年 10月 17日

所要時間::
02:56
How to use a single LSF device to translate between multiple voltages in the same system.

Other Logic Training Videos

Videos developed as training about logic and voltage translation; which still contain great information but don't fit into a videos series.

Overviews of Devices and EVMs

A collection of videos reviewing specific logic and voltage translation parts or EVMs, including their key features and specifications.
36 結果
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki