UCC5870-Q1 EVM Quick Start Demo
説明
2020年 6月 23日
This video gives a quick start demo for the UCC5870-Q1 EVM including:
- EVM hardware and the test system setup
- Initial programming of the driver
- How to power-up the EVM board
- Starting the GUI software and building up the connection between the GUI and the driver
- How to program the driver from reset state to configuration 1, 2 and active
When the driver is in active state, it can output PWM which follows the input PWM signal with example such as continuous PWM and double pulses PWM were given, how to generate desat fault and how to clear the fault was also explained).