Advanced Topics on the BQ40z80 - Current Scaling
설명
2018년 9월 20일
The BQ40z80 natively supports pack capacities up to 29Ah and battery currents up to 32A, and the BQ40z80 also includes a scale factor that can be set between 0 and 100 to “scale up” the currents seen by the coulomb counter. This video gives an overview of this function.
추가 정보
This course is also a part of the following series
Date: 10월 8일, 2018년