TI Training home
Near field communication (NFC)
Near Field Communication (NFC) Training Series Part 3: NFC Applications
Near field communication (NFC)
이메일
Near Field Communication (NFC) Training Series Part 3: NFC Applications
Now let's look at an overview of applications around the consumer. What you see on the right side are applications where the smartphone is typically using the card emulation mode. These are applications where an NFC device will replace a traditional RFID card. For example, access control and hotel room.
The smartphone is becoming your key to access your hotel room. You receive the authorization for the room onto your phone, and you only have to present the smartphone to the door lock system, and you can enter your room without stopping at the front desk and receiving a physical card.
Other applications where card emulation can be used are transport ticketing, event ticketing, and payments. On the left side here in red, you have applications that typically use the Reader/Writer mode, and where the smartphone can replace an RFID reader/writer. It also opens the possibilities for a lot of new applications, as it is now the first time the consumer has an RFID reader in their hand to readout transponders.
For product authentication, the NFC functionality in the smartphone enables you to make sure it's an authentic product if it is equipped with an NFC transponder. And at the same time, you can get additional information about the product you're about to purchase. It enables automatic configuration adjustments in your car and at home to your specific settings. And enables simplified pairing for Bluetooth and Wi-Fi connections, which is a completely new application, currently driving the implementation of NFC in a lot of end equipments. We will cover this specific application in the following slides in more detail.
The last operating mode, peer-to-peer, which enables specifically the communication of two smartphones with each other are used for content sharing, like business cards, phone numbers, apps, pictures, and music. To summarize the use case NFC is addressing, we see tap and identify, tap and pair, tap and share, and finally, tap and authenticate.
Let's look a little bit deeper into the tap and pair use case to simplify the wireless pairing process. Bluetooth and Wi-Fi has become a standard feature in all smartphones and tablets, allowing communication with Bluetooth or Wi-Fi-enabled headphones, speakers, cameras, watches, and other devices. But the pairing and set up process to the correct device can be troublesome and complicated. You have to go through different menus on your screen, have to enter long keys, and so on.
As an example, the Bluetooth process consists of setting the Bluetooth-enabled device into a discoverable mode, generally by pressing and holding a button for an extended period, then inquiring for devices within range on your phone or tablet, and selecting your device from a potentially long list. For Wi-Fi, it's even more complicated.
NFC can be used to simplify and enhance the user experience by removing the need for the inquiry process, and also allowing for a specific application to be opened after reading the NFC message-- all with only a tap. The close proximity of the two devices ensure that this is the exact device you are looking to pair. The NFC Forum and Bluetooth sig have collaborated on an application document titled Bluetooth Secure and Simple Pairing Using NFC, which provides examples and solidifies the message formatting for out-of-band pairing using NFC. The same has been established for Wi-Fi connection.
With only a touch, you can set up the wireless connection for Bluetooth or Wi-Fi. On the left side, you have an example for direct pairing. Pass the set-up parameters, handshake, and set up Bluetooth or Wi-Fi connection between the two devices directly. On the right side is an example for indirect pairing. In this case, the NFC-enabled mobile phone or tablet can be a transportation bridge to pass the set-up parameters between the consumer device and an access point.
An example would be if you want to connect a new printer to your router, your smartphone is already connected to your router, and can now give the required connection parameters through NFC to the new printer, which can afterwards, do the pairing process with the router. Or you want to install a new camera for your home security system. Instead of connecting it to your PC, going through all the set-up menus, you install it on the outside in the position that you'd like, come with your phone to transmit the pairing parameters through NFC. The camera automatically connects your router, and you can also open the app which shows you the picture from the camera on your phone-- all with one tap. After the NFC pairing process, the Bluetooth or Wi-Fi takes over, and the application proceeds transferring of audio, video, data, et cetera.
Another application is tap and share and using NFC as a service interface. We have talked a lot about applications around the consumer and what the consumer can now do with NFC-enabled smartphone in their hands. But the same is also possible in the professional environment, where the NFC-enabled smartphone eliminates the need for a specific handheld device. The NFC smartphone can be used as a universal display, an entry device for nearly any end equipment. This reduces the hardware BOM in the end equipment, and you get a high-resolution display and convenient touch screen.
You only have to connect through NFC over the short distance what gives you inherent security, and you can get the data out you need-- status information, counter readings, diagnostics, configuration data. Or you can also make far more updates to the end equipment if required. The use of wireless NFC communication gives great flexibility for the design, compared to an IR interface, where you need line-of-sight, or a wired interface, especially if you want to hermetically seal the end equipment.
Now let's have look to NFC in the context of the internet of things. Or let's even go one step further to the internet of everything. NFC can be the last step, the last few centimeters to connect a device, sensor, through NFC to the smartphone, and then transmit data with the smartphone to the internet. We are now combining the NFC technology with sensors as intelligent tags. We are enabling health and fitness, and medical systems. People can monitor their vital data with the health and fitness patches, and can share the collected data securely with their doctor or health providers. The doctor can provide immediate information back-- what they should do based on their health conditions.
It makes it easy. It makes it more convenient. You will more frequently monitor your health conditions when you do not have to go to the doctor, but you can get the direct feedback from the measurement results.
Also in the industrial area, NFC combined with sensors enables new possibilities, especially as it enables battery list sensors powered from the RF field of a smartphone or another NFC reader device. So monitoring of process parameters is possible, even in positions where it's difficult to have line power available or where you cannot have batteries, or replace batteries, on a continual basis. 现在我们来大致了解 消费类应用。 在右侧呈现的应用中 , 智能手机 通常采用卡仿真模式。 这些应用使用 NFC 器件 替代传统的 RFID 卡。 例如,宾馆房间的 进入控制。 智能手机逐渐成为您进入 宾馆房间的钥匙。 您的手机接收房间的授权信息 , ,只需将手机靠近门锁 系统即可进入, 无需 在前台 获取实体房卡。 其他可使用卡模式的应用 包括交通售票、 活动售票和付款。 左侧红色部分的应用通常 采用 读/写器模式,智能手机在该模式下 可以替代 RFID 读写器。 这也让众多新应用的问世变为可能 , 因为消费者首次可以 使用 掌中的 RFID 阅读器 读取应答器。 对于产品鉴定,智能手机中的 NFC 功能 允许用户 确保 这是一款经过验证并且配有 NFC 应答器的 可靠产品。 与此同时,还可以 了解所要 购买产品的详细信息。 它支持在汽车和家庭环境中 根据您的特定设置 自动调节相关配置。 同时简化了蓝牙 和 Wi-Fi 连接的配对过程,这种 全新应用当前 推动着 NFC 应用于 众多终端设备。 我们将在后续的幻灯片中详细介绍 这种 特定应用。 最后一种操作 模式,即点对点模式, 专门支持两部 智能手机间的通信, 适用于共享 名片、 电话号码、应用程序 、 图片和音乐等内容。 为了总结应用 NFC 的用例 , 我们分为点击识别、 点击配对、点击共享 以及 点击身份验证。 我们来深入了解 简化无线 配对过程的点击配对用例。 蓝牙和 Wi-Fi 已 成为 所有智能手机 和平板电脑中的标准功能,允许 其与支持蓝牙 或 Wi-Fi 功能的 耳机、扬声器、摄像机、 手表及其他设备进行通信。 但与正确设备的配对和设置过程 较为麻烦 和复杂。 用户必须浏览 屏幕中的不同菜单, 输入冗长的 密钥并完成其他操作。 例如, 蓝牙的过程为 通常按住一个按钮较长时间,将 支持蓝牙功能的设备 设置为可发现 模式, 然后查询手机或平板电脑 范围内的设备 ,最后从 可能很长的 设备名单中选择所需设备。 对于 Wi-Fi,该过程 更为复杂。 NFC 可免去查询过程并支持在 读取 NFC 消息后打开特定应用程序 , 从而简化操作并增强 用户体验 - 指尖轻触设备即可完成所有操作。 两台设备足够接近 可确保精确 定位需要配对的设备。 NFC 论坛和蓝牙技术联盟 合作 发表了名为《使用 NFC 的蓝牙安全简易配对》 的应用文档 , 其中提供了相关示例并确定了 使用 NFC 进行带外 配对的消息格式。 Wi-Fi 连接同样建立了 相关机制。 轻触指尖即可建立 蓝牙 或 Wi-Fi 连接。 左侧为 直接配对示例。 传输设置参数 、完成握手并 在两设备间建立蓝牙或 Wi-Fi 连接。 右侧为 间接配对示例。 在这种情况下,支持 NFC 的 手机或平板电脑 可为消费者设备 与接入点 传输设置参数 的桥梁。 例如您需要将打印机与路由器相连 , 智能手机 s已经与路由器 相连并将 所需连接参数 通过 NFC 发送至 新打印机 。 此后,该打印机 将与路由器配对。 或者在家庭安全系统中安置 一个新的摄像机。 您将摄像机放置在 室外的指定位置, 使用手机通过 NFC 传输 配对参数 , 无需将其 连接 电脑并浏览所有设置菜单。 摄像机与 路由器自动相连, 您可以通过应用程序 在手机上查看摄像机 拍摄的画面 -- 轻触指尖即可完成所有操作。 完成 NFC 配对过程后 ,蓝牙或 Wi-Fi 进行接管,应用程序 执行 音频、 视频及数据等内容的传输操作。 下一种应用是点击共享应用 , 使用 NFC 作为 服务接口。 我们讨论了很多 有关消费类 应用的内容以及 消费者 可以使用掌中支持 NFC 功能 的智能手机所完成的操作。 但专业环境中也可能存在相同情况 , 在其中使用支持 NFC 的 智能手机时 无需使用特定手持设备。 NFC 智能手机可用作 通用显示屏, 适用于几乎所有 终端设备的输入设备。 这减少了终端设备的 硬件 BOM ,可以获得一款高分辨率显示屏 以及便捷的触摸 屏幕。 您仅需在确保固有安全性的短距离内 通过 NFC 进行连接, 即可获取所需 数据, 包括状态信息 、计数器读数、诊断和 配置数据。 或者,您还可以根据需要继续深入 更新终端设备。 对于需要视距或有线接口 , 尤其适用于采用密封封装的 终端设备, 与 IR 接口相比 , 使用无线 NFC 通信 赋予 设计巨大灵活性。 现在介绍 NFC 在 物联网领域的应用。 或者进一步 了解物联网。 NFC 是在几厘米距离内 将设备、传感器通过 NFC 与智能手机相连的最后一步 , 然后通过 智能手机将数据传输至互联网。 我们正将 NFC 技术与 传感器相结合, 构成 智能标签。 我们支持健康与 保健以及医疗系统。 用户可以通过健康和保健贴片 监测身体的重要数据 , 并与医生和医疗保健服务方 安全共享。 医生可以提供 即时信息, 根据用户健康状况 ,告知其应采取的措施。 它让一切易如反掌。 它让一切便利快捷。 在不必拜访医生时,您能够时常 监控健康状况 , 根据测量结果可 直接获得反馈。 此外在工业领域, NFC 与传感器相结合 提供了新的契机 ,尤其是 因为它支持电池 光传感器 由智能手机 或其他 NFC 阅读器 设备的 RF 场供电。 因此,即使处于难以提供 线路功率的位置、没有电池或 无法持续更换电池 , 也可以 监测过程参数。 现在我们来大致了解 消费类应用。 在右侧呈现的应用中 , 智能手机 通常采用卡仿真模式。 这些应用使用 NFC 器件 替代传统的 RFID 卡。 例如,宾馆房间的 进入控制。 智能手机逐渐成为您进入 宾馆房间的钥匙。 您的手机接收房间的授权信息 , ,只需将手机靠近门锁 系统即可进入, 无需 在前台 获取实体房卡。 其他可使用卡模式的应用 包括交通售票、 活动售票和付款。 左侧红色部分的应用通常 采用 读/写器模式,智能手机在该模式下 可以替代 RFID 读写器。 这也让众多新应用的问世变为可能 , 因为消费者首次可以 使用 掌中的 RFID 阅读器 读取应答器。 对于产品鉴定,智能手机中的 NFC 功能 允许用户 确保 这是一款经过验证并且配有 NFC 应答器的 可靠产品。 与此同时,还可以 了解所要 购买产品的详细信息。 它支持在汽车和家庭环境中 根据您的特定设置 自动调节相关配置。 同时简化了蓝牙 和 Wi-Fi 连接的配对过程,这种 全新应用当前 推动着 NFC 应用于 众多终端设备。 我们将在后续的幻灯片中详细介绍 这种 特定应用。 最后一种操作 模式,即点对点模式, 专门支持两部 智能手机间的通信, 适用于共享 名片、 电话号码、应用程序 、 图片和音乐等内容。 为了总结应用 NFC 的用例 , 我们分为点击识别、 点击配对、点击共享 以及 点击身份验证。 我们来深入了解 简化无线 配对过程的点击配对用例。 蓝牙和 Wi-Fi 已 成为 所有智能手机 和平板电脑中的标准功能,允许 其与支持蓝牙 或 Wi-Fi 功能的 耳机、扬声器、摄像机、 手表及其他设备进行通信。 但与正确设备的配对和设置过程 较为麻烦 和复杂。 用户必须浏览 屏幕中的不同菜单, 输入冗长的 密钥并完成其他操作。 例如, 蓝牙的过程为 通常按住一个按钮较长时间,将 支持蓝牙功能的设备 设置为可发现 模式, 然后查询手机或平板电脑 范围内的设备 ,最后从 可能很长的 设备名单中选择所需设备。 对于 Wi-Fi,该过程 更为复杂。 NFC 可免去查询过程并支持在 读取 NFC 消息后打开特定应用程序 , 从而简化操作并增强 用户体验 - 指尖轻触设备即可完成所有操作。 两台设备足够接近 可确保精确 定位需要配对的设备。 NFC 论坛和蓝牙技术联盟 合作 发表了名为《使用 NFC 的蓝牙安全简易配对》 的应用文档 , 其中提供了相关示例并确定了 使用 NFC 进行带外 配对的消息格式。 Wi-Fi 连接同样建立了 相关机制。 轻触指尖即可建立 蓝牙 或 Wi-Fi 连接。 左侧为 直接配对示例。 传输设置参数 、完成握手并 在两设备间建立蓝牙或 Wi-Fi 连接。 右侧为 间接配对示例。 在这种情况下,支持 NFC 的 手机或平板电脑 可为消费者设备 与接入点 传输设置参数 的桥梁。 例如您需要将打印机与路由器相连 , 智能手机 s已经与路由器 相连并将 所需连接参数 通过 NFC 发送至 新打印机 。 此后,该打印机 将与路由器配对。 或者在家庭安全系统中安置 一个新的摄像机。 您将摄像机放置在 室外的指定位置, 使用手机通过 NFC 传输 配对参数 , 无需将其 连接 电脑并浏览所有设置菜单。 摄像机与 路由器自动相连, 您可以通过应用程序 在手机上查看摄像机 拍摄的画面 -- 轻触指尖即可完成所有操作。 完成 NFC 配对过程后 ,蓝牙或 Wi-Fi 进行接管,应用程序 执行 音频、 视频及数据等内容的传输操作。 下一种应用是点击共享应用 , 使用 NFC 作为 服务接口。 我们讨论了很多 有关消费类 应用的内容以及 消费者 可以使用掌中支持 NFC 功能 的智能手机所完成的操作。 但专业环境中也可能存在相同情况 , 在其中使用支持 NFC 的 智能手机时 无需使用特定手持设备。 NFC 智能手机可用作 通用显示屏, 适用于几乎所有 终端设备的输入设备。 这减少了终端设备的 硬件 BOM ,可以获得一款高分辨率显示屏 以及便捷的触摸 屏幕。 您仅需在确保固有安全性的短距离内 通过 NFC 进行连接, 即可获取所需 数据, 包括状态信息 、计数器读数、诊断和 配置数据。 或者,您还可以根据需要继续深入 更新终端设备。 对于需要视距或有线接口 , 尤其适用于采用密封封装的 终端设备, 与 IR 接口相比 , 使用无线 NFC 通信 赋予 设计巨大灵活性。 现在介绍 NFC 在 物联网领域的应用。 或者进一步 了解物联网。 NFC 是在几厘米距离内 将设备、传感器通过 NFC 与智能手机相连的最后一步 , 然后通过 智能手机将数据传输至互联网。 我们正将 NFC 技术与 传感器相结合, 构成 智能标签。 我们支持健康与 保健以及医疗系统。 用户可以通过健康和保健贴片 监测身体的重要数据 , 并与医生和医疗保健服务方 安全共享。 医生可以提供 即时信息, 根据用户健康状况 ,告知其应采取的措施。 它让一切易如反掌。 它让一切便利快捷。 在不必拜访医生时,您能够时常 监控健康状况 , 根据测量结果可 直接获得反馈。 此外在工业领域, NFC 与传感器相结合 提供了新的契机 ,尤其是 因为它支持电池 光传感器 由智能手机 或其他 NFC 阅读器 设备的 RF 场供电。 因此,即使处于难以提供 线路功率的位置、没有电池或 无法持续更换电池 , 也可以 监测过程参数。
설명
2015년 6월 16일
This is the third of five videos in the NFC training series. This presentation highlights the various NFC operating modes and dives deeper into the supported application areas.