TI Training home
Near field communication (NFC)
Near Field Communication (NFC) Training Series Part 5: NFC Markets and TI Offering
Near field communication (NFC)
이메일
Near Field Communication (NFC) Training Series Part 5: NFC Markets and TI Offering
If we look now into the different market segments where NFC can be used, the first is the consumer electronics space, where especially pairing applications with printers, routers, cameras, and wireless audio equipment are now driving the integration of NFC into a lot of different devices. In the automotive area, we see more and more of the integration of NFC into the infotainment system, or the combination with a wireless charging system, also to enable easy pairing with a smartphone. Another use case in the automotive area is for car-sharing systems, where you can get authorization for a car to the smartphone, and then use the NFC functionality to open the car.
In the industrial space, the applications are very broad, with the use of NFC as service or configuration interface, where it can be more or less integrated into any kind of equipment and enable communication with a smartphone. In the retail segment, it is the payment application for which NFC is now used, and for which it was originally developed. In retail, NFC is also used for product authentication of an original product, and gating additional product information.
In the Smart Grid market, we have two areas. One is the prepayment application, where you can now use an NFC-enabled phone for prepayment, instead of an RFID card. And the other is the service interface, like in industrial segments, as a lot of the meters need to be hermetically sealed.
The last segment is medical, where NFC enables phones in the hands of the consumers' completely new applications for self-monitoring, in combination with medical and bio-patches, and other mobile measurement equipment which can be connected through NFC to a smartphone.
We are matching the TI products to the market segments. We see that the RF 430CL330H is used in the consumer and automotive market, mainly to simplify the pairing of an alternative carrier, like Bluetooth or Wi-Fi. And in the industrial and Smart Grid market, it's used as a service and configuration interface.
The TRF796X and TRF7970A are used in automotive for the access to the car, car-sharing applications, in industrial applications, as a reader/writer device, where the smartphone is in Card Emulation mode, like a door lock system, or in applications where, also, the Peer-to-Peer mode needs to be supported.
In the medical area, the RF430FRL152H enables medical patches, and can also be used in the industrial space for logistics applications, like food tracking, where constant temperature monitoring is required.
Coming now to the ecosystem to support the development-- we have a broad portfolio of development boards, ranging from standalone evaluation kits to target board and booster packs which can be used in combination with the different microcontroller development platforms. Embedded firmware is fully integrated into TI's Code Composer Studio and IAR's Embedded Workbench integrated development environment systems.
Comprehensive documentation and TI designs with all design files are also provided for reference. Additional information can be found under www.TI.com/NFC. On the product folders of the individual products, the data sheets, technical reference manuals, application notes, software code are all available for download. We also have several short training videos available and link to the E2E Forum to ask questions and exchange information with a broad community of experts. It's also included in this slide.
TI has been active in the RFID market for more than 25 years, and has delivered more than one billion transponder and reader products to the market. We have participated, guided, and influenced the definitions of the NFC specifications from the beginning, and are a member of the NFC Forum and the ISO Standardization groups, and actively working in different task forces, working groups, and committees.
We are continually developing highly differentiated products by integrating low-power RF wireless technologies, together with ultra-low-power microcontrollers, advanced FRAM memory technology, security functions, and sensors to enable our customers to design innovative system solutions.
With NFC, the possibilities are endless to create innovative solutions in various markets. From a technology side, NFC is a short-range radio technology that enables bi-directional communication, where one side can be battery-less, powered from the other side.
From a use case side, NFC can be used as a universal service and configuration interface for nearly every end-equipment. It is not always a question if you use the one or other wireless technology. NFC can also be combined with other wireless technologies and enable easy pairing for Bluetooth, BLE, and Wi-Fi. NFC can provide the final link for sensors, nodes, medical patches, to connect them to the Internet of Things.
But NFC is also not the wireless solution for every application. It has very specific characteristics, like the dedicated read zone and battery-less operation, which can be used to automate processes for consumer, industrial, and medical applications. Thanks for watching. 如果我们现在来研究一下 可以应用近场通信 (NFC) 的 不同细分市场, 那么首先要提的便是消费类电子领域, 尤其是与打印机、路由器、摄像机 和无线音频设备配对的 应用目前正在推动着 NFC 集成到 众多不同 设备中。 在汽车领域, 越来越多的 NFC 融入 信息娱乐系统或 与无线充电系统 搭配使用, 他们也能够 与智能手机轻松配对。 汽车领域的另一项用例是 应用于汽车共享系统, 您可以通过智能手机 获取汽车授权 然后使用 NFC 功能 打开车门。 在工业领域中, 使用 NFC 作为服务或 配置接口的应用非常广泛。 NFC 或多或少地在 各种设备中集成 并支持与智能手机进行通信。 在零售业细分市场,NFC 现应用于 支付应用。 这也是 NFC 的 开发初衷。 在零售业领域,NFC 还用于 原产品的身份验证 以及收集 更多有关产品 的信息.
在智能电网市场,NFC 应用于 两个领域。 其中一个领域是预付款 应用, 您可以使用支持 NFC 的 手机取代 射频识别 (RFID) 卡预付账款。 另一个领域是 服务接口, 与工业领域相似 , 许多电表需要采用密封封装。 最后一个细分市场 是医疗。 NFC 支持通过手机掌控 消费者的全新应用 ,与医疗和生物贴片以及可通过 NFC 与智能手机相连的 其他 移动测量设备相结合, ,以进行 自我监测。 我们正将 TI 产品 应用于匹配的细分市场。 RF 430CL330H 应用于消费类和汽车市场, 主要目的是 简化 非传统信息载体 (如蓝牙或 Wi-Fi)的配对。 在工业和 智能电网市场, NFC 用作服务和 配置接口。 TRF796X 和 TRF7970A 在汽车领域用于 汽车访问、汽车共享应用 , 在工业应用中用作读/写器 , 其中智能手机处于 卡仿真模式(如门锁系统), ,第三种是还需支持 点对点模式的应用。 在医疗领域, RF430FRL152H 应用于医疗 贴片, 还可用于工业领域的 逻辑应用, 如需要 恒温监测的食品跟踪应用。 现在介绍支持发展的生态系统 — 我们提供众多开发板产品组合 , 范围遍及独立评估套件到 目标板和 BoosterPack 应用于 不同微控制器 开发平台中。 嵌入式固件在 TI 的 Code Composer Studio 以及 IAR Embedded Workbench 集成 开发环境中完全集成。 提供全面的文档 及 TI 参考设计(附带所有设计文件) 进行参考。 更多相关信息,请访问 www.TI.com/NFC。 各产品文件夹中提供的 所有 数据表、技术参考手册、应用 手册、 软件代码 均可下载。 我们还提供多部简短的培训视频并 链接至 E2E 论坛 , 便于您向众多 社区专家提问和沟通交流。 这些内容也在 幻灯片中进行了介绍。 TI 在 25 年多的时间里致力于 RFID 市场 , 供应了超过 10 亿个 应答器和 阅读器产品。 我们在初始阶段参与、 指导并影响了 NFC 规范的定义 ,隶属于 NFC 论坛和 国际标准化组织 , 活跃在不同的 任务组、 工作组和委员会。 通过将低功耗 RF 无线技术与 超低功耗微控制器、 高级 FRAM 存储器技术、安全功能和传感器相集成 , 我们持续开发与众不同的产品 , 支持消费者设计创新性 系统解决 方案。 NFC 令在众多市场中创建 创新解决方案 充满无限可能。 从技术角度出发,NFC 是 一种短距离无线电技术, 支持一侧采用无电池设计 , 而由另一侧供电 的双向通信。 从用例角度出发,NFC 可 用作几乎所有终端设备的 通用服务 和配置接口。 使用这种 或其他无线技术不会始终存在问题。 NFC 也可与 其他无线技术相结合, 轻松与 蓝牙、BLE 和 Wi-Fi 配对。 NFC 可提供 传感器、节点、医疗贴片的 最终链接, 将其与 物联网相连。 但 NFC 并非所有应用的无线 解决方案。 它具备非常具体的 特性 (如专用读取区 和无电池运行), 可用于实现 消费类、工业和医疗应用的 过程自动化。 谢谢观看。 如果我们现在来研究一下 可以应用近场通信 (NFC) 的 不同细分市场, 那么首先要提的便是消费类电子领域, 尤其是与打印机、路由器、摄像机 和无线音频设备配对的 应用目前正在推动着 NFC 集成到 众多不同 设备中。 在汽车领域, 越来越多的 NFC 融入 信息娱乐系统或 与无线充电系统 搭配使用, 他们也能够 与智能手机轻松配对。 汽车领域的另一项用例是 应用于汽车共享系统, 您可以通过智能手机 获取汽车授权 然后使用 NFC 功能 打开车门。 在工业领域中, 使用 NFC 作为服务或 配置接口的应用非常广泛。 NFC 或多或少地在 各种设备中集成 并支持与智能手机进行通信。 在零售业细分市场,NFC 现应用于 支付应用。 这也是 NFC 的 开发初衷。 在零售业领域,NFC 还用于 原产品的身份验证 以及收集 更多有关产品 的信息. 在智能电网市场,NFC 应用于 两个领域。 其中一个领域是预付款 应用, 您可以使用支持 NFC 的 手机取代 射频识别 (RFID) 卡预付账款。 另一个领域是 服务接口, 与工业领域相似 , 许多电表需要采用密封封装。 最后一个细分市场 是医疗。 NFC 支持通过手机掌控 消费者的全新应用 ,与医疗和生物贴片以及可通过 NFC 与智能手机相连的 其他 移动测量设备相结合, ,以进行 自我监测。 我们正将 TI 产品 应用于匹配的细分市场。 RF 430CL330H 应用于消费类和汽车市场, 主要目的是 简化 非传统信息载体 (如蓝牙或 Wi-Fi)的配对。 在工业和 智能电网市场, NFC 用作服务和 配置接口。 TRF796X 和 TRF7970A 在汽车领域用于 汽车访问、汽车共享应用 , 在工业应用中用作读/写器 , 其中智能手机处于 卡仿真模式(如门锁系统), ,第三种是还需支持 点对点模式的应用。 在医疗领域, RF430FRL152H 应用于医疗 贴片, 还可用于工业领域的 逻辑应用, 如需要 恒温监测的食品跟踪应用。 现在介绍支持发展的生态系统 — 我们提供众多开发板产品组合 , 范围遍及独立评估套件到 目标板和 BoosterPack 应用于 不同微控制器 开发平台中。 嵌入式固件在 TI 的 Code Composer Studio 以及 IAR Embedded Workbench 集成 开发环境中完全集成。 提供全面的文档 及 TI 参考设计(附带所有设计文件) 进行参考。 更多相关信息,请访问 www.TI.com/NFC。 各产品文件夹中提供的 所有 数据表、技术参考手册、应用 手册、 软件代码 均可下载。 我们还提供多部简短的培训视频并 链接至 E2E 论坛 , 便于您向众多 社区专家提问和沟通交流。 这些内容也在 幻灯片中进行了介绍。 TI 在 25 年多的时间里致力于 RFID 市场 , 供应了超过 10 亿个 应答器和 阅读器产品。 我们在初始阶段参与、 指导并影响了 NFC 规范的定义 ,隶属于 NFC 论坛和 国际标准化组织 , 活跃在不同的 任务组、 工作组和委员会。 通过将低功耗 RF 无线技术与 超低功耗微控制器、 高级 FRAM 存储器技术、安全功能和传感器相集成 , 我们持续开发与众不同的产品 , 支持消费者设计创新性 系统解决 方案。 NFC 令在众多市场中创建 创新解决方案 充满无限可能。 从技术角度出发,NFC 是 一种短距离无线电技术, 支持一侧采用无电池设计 , 而由另一侧供电 的双向通信。 从用例角度出发,NFC 可 用作几乎所有终端设备的 通用服务 和配置接口。 使用这种 或其他无线技术不会始终存在问题。 NFC 也可与 其他无线技术相结合, 轻松与 蓝牙、BLE 和 Wi-Fi 配对。 NFC 可提供 传感器、节点、医疗贴片的 最终链接, 将其与 物联网相连。 但 NFC 并非所有应用的无线 解决方案。 它具备非常具体的 特性 (如专用读取区 和无电池运行), 可用于实现 消费类、工业和医疗应用的 过程自动化。 谢谢观看。
설명
2015년 6월 16일
This is the final video in the NFC training series. This presentation covers the various market segments and tools available to help you get started with your NFC design.