2018 South Asia Industrial webinar series

Email

6.1 Overview of commonly-used interface for industrial application Part 1

Description

December 19, 2018

The training provides a very comprehensive introduction of the commonly-used interface including RS-485, RS-422, ProfiBus, RS-232, IO-Link, CAN and LIN. These interfaces are used in the application of Factory Automation and some other industrial application. For the engineer who needs to deal with interface system design, this is a very useful training.

Part 1: First the speaker shows the communication hierarchy of all the interface type and how it impact on the communication design. Then the training further introduces the RS-485 and how it works in the system.

Additional information

arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki