Processor SDK Training Series
TI provides key runtime software components and documentation to further ease development. TI’s online training provides an introduction to the Processor SDK and how to use this software to start building applications on TI embedded processors.
Table of contents
Additional information
For more information on AM57x Sitara processors, refer to the AM57x Sitara™ Processors Training Series.
For more information on TI ARM & DSP processors, refer to the KeyStone ARM & DSP Multicore Device Training Series
For a high-level look at the AM57x Sitara evaluation module, view the Evaluate the New AM57x Sitara Processors with an EVM Based on the New BeagleBoard-X15 video.
1. Processor SDK for TI Embedded Processors
# | Title | Duration | ||
---|---|---|---|---|
1.1 |
Introduction to the Processor SDK Training Series
This short video provides an introduction of the Processor SDK training series including how to access and a curriculum overview.
|
02:32 | This short video provides an introduction of the Processor SDK training series including how to access and a curriculum overview. | |
1.2 |
Processor SDK Overview
This module provides an introduction to the Processor Software Development Kit (SDK), the next generation unified software platform for TI’s newest processor...
|
This module provides an introduction to the Processor Software Development Kit (SDK), the next generation unified software platform for TI’s newest processor... | ||
1.3 |
Introduction to Processor SDK RTOS Part 1
This module is the first installment of a two-part overview of the Processor SDK from the TI-RTOS perspective. It introduces the functional elements that...
|
This module is the first installment of a two-part overview of the Processor SDK from the TI-RTOS perspective. It introduces the functional elements that... | ||
1.4 |
Introduction to Processor SDK RTOS Part 2
This module is the second installment of a two-part overview of the Processor SDK from the TI-RTOS perspective. It examines the functional elements that...
|
This module is the second installment of a two-part overview of the Processor SDK from the TI-RTOS perspective. It examines the functional elements that... | ||
1.5 |
Application Development Using Processor SDK RTOS
This presentation provides a detailed overview of the application development process using the Processor SDK RTOS release. It walks through each step...
|
This presentation provides a detailed overview of the application development process using the Processor SDK RTOS release. It walks through each step... | ||
1.6 |
Processor SDK Linux Overview
This module takes a look at the purpose of the Processor SDK for Linux, how it is designed to provide flexibility and re-usability, and how the kit creates...
|
This module takes a look at the purpose of the Processor SDK for Linux, how it is designed to provide flexibility and re-usability, and how the kit creates... | ||
1.7 |
Processor SDK Linux Components
This module provides an introduction to the functional components included in the Processor SDK for Linux and describes how these components can be used...
|
This module provides an introduction to the functional components included in the Processor SDK for Linux and describes how these components can be used... | ||
1.8 |
Processor SDK Linux Matrix Application Launcher Overview
This module explains the purpose of the Matrix, an example application that launches by default within the Processor SDK for Linux. The capabilities of...
|
This module explains the purpose of the Matrix, an example application that launches by default within the Processor SDK for Linux. The capabilities of... | ||
1.9 |
Processor SDK Linux Installation, Documentation, and Training
This module identifies the resources needed to obtain and install the Processor SDK for Linux. It also provides an overview of supporting documentation...
|
This module identifies the resources needed to obtain and install the Processor SDK for Linux. It also provides an overview of supporting documentation... | ||
1.10 |
Introduction to OpenCL on TI Embedded Processors
This module provides an overview of OpenCL, the benefits it can provide during application development, and the criteria to consider for using OpenCL on...
|
This module provides an overview of OpenCL, the benefits it can provide during application development, and the criteria to consider for using OpenCL on... | ||
1.11 |
Introduction to Inter-Processor Communication (IPC) for KeyStone and Sitara™ Devices
The IPC software package is designed to hide the lower-layer hardware complexity of multi-core devices and help users to quickly develop applications
|
The IPC software package is designed to hide the lower-layer hardware complexity of multi-core devices and help users to quickly develop applications | ||
1.12 |
Setting Up and Testing Processor SDK RTOS Device Drivers
This video demonstrates how to setup and test device drivers included in the Processor SDK RTOS package.
|
05:44 | This video demonstrates how to setup and test device drivers included in the Processor SDK RTOS package. | |
1.13 |
Introduction to the Sitara™ AM57x Processor Industrial Software Development
This training provide an overview of the AM57x Industrial SDK architecture.
|
This training provide an overview of the AM57x Industrial SDK architecture. |