Hint: separate multiple terms with commas

E.g., 02/18/2019

E.g., 02/18/2019

Hint: separate multiple terms with commas

E.g., 02/18/2019

E.g., 02/18/2019

Sort by:

274 Results

SimpleLink™ Academy - POSIX Project Zero

When: March 9, 2017
POSIX (Portable Operating System Interface) is an IEEE industry API standard for OS compatibility. The SimpleLink™ software development kits (SDKs) has both TI-RTOS and FreeRTOS support, however it also offers POSIX support on top of either of these RTOS's. This allows applications to be independent of the underlying RTOS. This workshop provides a simple introduction to using POSIX with the SimpleLink SDK. You will use TI Resource Explorer, the SimpleLink SDK, and CCS Cloud to modify a project and run it on a SimpleLink LaunchPad™ Development Kit. The goal for this project is to familiarize you with some POSIX APIs and concepts typically used in multithreaded applications. This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible.     

SimpleLink™ Academy - TI Drivers | MSP432 Single-Threaded ADC

When: March 9, 2017
This lab introduces the use of the SimpleLink SDK to build a single-threaded (single-task) example using the MSP432 precision ADC. The lab uses TI-RTOS through POSIX API calls for all OS functions, such as thread and semaphore setup. This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible.

SimpleLink™ Academy - TI Drivers | Multi-threaded RTOS Thermostat

When: March 9, 2017
This lab introduces multi-threading (multi-tasking) with the SimpleLink SDK. In the example project, we build a thermostat using POSIX API calls with TI-RTOS on an MSP432 LaunchPad with the Sensors BoosterPack.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - TI Drivers | Using GUI Composer JTAG/XDS model

When: March 9, 2017
This workshop is a continuation of the TI Drivers Project Zero exercise. We will expand on that example by creating a simple PC-side graphical user interface (GUI) that complements our example. If you remember, we created a simple application that continually reads an ADC channel & toggles an LED on or off depending on whether or not our ADC reading exceeds a threshold.To do this, we will use a nifty tool called GUI Composer. GUI Composer is a browser-based utility for creating PC-side graphical interfaces for interacting with your hardware. GUI Composer supports several interfaces today, including Serial/UART, JTAG/XDS, or MQTT (for IoT applications).This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible.

SimpleLink™ Academy - TI Drivers | GPIO Interrupt

When: March 9, 2017
This workshop is a simple introduction for setting up GPIO interrupts using TI Drivers within the Simplelink™ SDK. We will be leveraging the gpio_interrupt code example provided within the SimpleLink SDK for reference.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible.

SimpleLink™ Academy - TI Drivers | Porting TI Drivers

When: March 9, 2017
With changing markets and new devices always coming out, software should be written in a manner which allows it to be moved to different devices easily. With the SimpleLink™ software development kits (SDKs), no/minimal application software changes are required when porting to a new device or RTOS. This is accomplished by using TI Drivers and POSIX APIs.This workshop is an introduction to the portability of applications using SimpleLink SDKs. This workshop will focus on the key areas that might be affected when porting an existing driver application to a different SimpleLink device.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - TI Drivers | Configuring TI Drivers

When: March 9, 2017
This workshop will dive into the details on how to configure TI Drivers for all SimpleLink Devices. We'll use these different devices in this workshop but the concepts are the same for all TI Drivers on all SimpleLink devices.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - TI-RTOS | Basic

When: March 9, 2017
TI-RTOS accelerates development schedules by eliminating the need to create basic system software functions from scratch. TI-RTOS scales from a minimal footprint real-time multitasking kernel - TI-RTOS Kernel (formerly known as SYS/BIOS) - to a complete RTOS solution including protocol stacks, multicore communications, device drivers and power management. By providing essential system software components pre-tested and pre-integrated, TI-RTOS enables developers to focus on differentiating their application.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 
SimpleLink Academy for MSP432

SimpleLink™ Academy for MSP432 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink MSP432 Host MCU.

SimpleLink™ Academy - Bluetooth LE | Fundamentals

When: March 9, 2017
This workshop is an introduction to the SimpleLink™ Bluetooth® low energy CC2640R2 software development kit (SDK) The 4 tasks in this lab session are targeted to be completed within a 2h time frame. There should be an intermediate level of knowledge of the C programming language as well experience with embedded software development to be able to complete the tasks.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - Bluetooth LE | Bluetooth Developer Studio

When: March 9, 2017
Learn how to use the Bluetooth Developer Studio GUI by Bluetooth SIG and the TI Code Generator plugin to accelerate the development of your own custom services This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - Bluetooth LE | Custom Profile

When: March 9, 2017
Explanation of the GATT and ATT protocols that Bluetooth Low Energy data exchange is based on, a walk-through of how to implement a custom Bluetooth service using the APIs provided in the TI BLE SDK, and a basic code generator for custom servicesThis training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - Bluetooth LE | Bluetooth Low Energy + Sensors BoosterPack

When: March 9, 2017
Learn how to port between devices in the SimpleLink family to read temperature data on the Simplelink CC2640R2 Wireless MCU. Enhance Project Zero by adding the ability to read and send temperature data over BLE.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible.

SimpleLink™ Academy - POSIX Project Zero

When: March 9, 2017
POSIX (Portable Operating System Interface) is an IEEE industry API standard for OS compatibility. The SimpleLink™ software development kits (SDKs) has both TI-RTOS and FreeRTOS support, however it also offers POSIX support on top of either of these RTOS's. This allows applications to be independent of the underlying RTOS.This workshop provides a simple introduction to using POSIX with the SimpleLink SDK. You will use TI Resource Explorer, the SimpleLink SDK, and CCS Cloud to modify a project and run it on a SimpleLink LaunchPad™ Development Kit. The goal for this project is to familiarize you with some POSIX APIs and concepts typically used in multithreaded applications.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - TI Drivers | Project Zero

When: March 9, 2017
This workshop is a simple introduction for using TI Drivers within the Simplelink™ SDK. To get our feet wet, we are going to start basic & will learn how to blink an LED on our LaunchPad using the SimpleLink SDK. Specifically, we are going to be using "TI Drivers", a collection of easy-to-use APIs that provide abstracted, functional access to various peripherals. Note that TI Drivers are compatible across the entire portfolio SimpleLink MCU devices.  This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible.     

SimpleLink™ Academy - TI Drivers | Using GUI Composer JTAG/XDS model

When: March 9, 2017
This workshop is a continuation of the TI Drivers Project Zero exercise. We will expand on that example by creating a simple PC-side graphical user interface (GUI) that complements our example. If you remember, we created a simple application that continually reads an ADC channel & toggles an LED on or off depending on whether or not our ADC reading exceeds a threshold.To do this, we will use a nifty tool called GUI Composer. GUI Composer is a browser-based utility for creating PC-side graphical interfaces for interacting with your hardware. GUI Composer supports several interfaces today, including Serial/UART, JTAG/XDS, or MQTT (for IoT applications).This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible.

SimpleLink™ Academy - TI Drivers | GPIO Interrupt

When: March 9, 2017
This workshop is a simple introduction for setting up GPIO interrupts using TI Drivers within the Simplelink™ SDK. We will be leveraging the gpio_interrupt code example provided within the SimpleLink SDK for reference.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible.  

SimpleLink™ Academy - TI Drivers | Porting TI Drivers

When: March 9, 2017
With changing markets and new devices always coming out, software should be written in a manner which allows it to be moved to different devices easily. With the SimpleLink™ software development kits (SDKs), no/minimal application software changes are required when porting to a new device or RTOS. This is accomplished by using TI Drivers and POSIX APIs.This workshop is an introduction to the portability of applications using SimpleLink SDKs. This workshop will focus on the key areas that might be affected when porting an existing driver application to a different SimpleLink device.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - TI Drivers | Configuring TI Drivers

When: March 9, 2017
This workshop will dive into the details on how to configure TI Drivers for all SimpleLink Devices. We'll use these different devices in this workshop but the concepts are the same for all TI Drivers on all SimpleLink devices.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - TI-RTOS | Basic

When: March 9, 2017
TI-RTOS accelerates development schedules by eliminating the need to create basic system software functions from scratch. TI-RTOS scales from a minimal footprint real-time multitasking kernel - TI-RTOS Kernel (formerly known as SYS/BIOS) - to a complete RTOS solution including protocol stacks, multicore communications, device drivers and power management. By providing essential system software components pre-tested and pre-integrated, TI-RTOS enables developers to focus on differentiating their application.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 
274 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki