Filters in use:
Filters in use:
Filters in use:
Filters in use:
Filters in use:
Sort by:
Isolation in Industrial Systems
In 2019 more than 2.5 million industrial robots will be in operation worldwide, according to a forecast of the international federation of robotics. An industrial robot typically consists out of a control cabinet, a robot arm and a Human Machine Interface (HMI) Panel. To guarantee safe operation of the complete robot system, the different robot components and its interfaces need to be isolated to each other.
Isolated Power Supplies for PLC I/O Modules
The training starts with an overview of an analog input module. Typical components and their voltage supply levels are shown. Next, possible power topologies like push-pull, flyback or flybuck with their advantages and disadvantages are discussed.
How to add Industrial Ethernet to Computer Numeric Control (CNC) Router Machine
CNC routers use step and direction signals to control each stepper motors. In addition motor information (position, temperature, fault) gets transferred from stepper motors back to control unit. This must be done in star topology and a mix of proprietary interfaces. Simple open real-time Ethernet (SORTE) enables 4 µs cycle time on industrial Ethernet and replaces step/direction signal and motor feedback info into a single Ethernet cable that is also wired in line topology.
Learn Different Solutions to Design a Field Transmitter Ultrasonic AFE
A common method to measure process parameters in plants is based on sound waves. This method is used in: level, flow and displacement field transmitters. It works based on measuring the time of flight (ToF) between when the pulse, generated by a piezo electric crystal, is sent and received back by the piezo.
Designing a Multi-Channel 4-20mA Analog Input Module
This training helps to understand relevant parameter of a 4-20mA analog input module, such as surge protection, handling miss-wiring, broken wire detection, isolation or protection of the module against over-current at power and signal inputs.
Design, Protection, and Technologies for Analog Outputs
Analog outputs in industrial automation come in a variety of configurations that each must deliver strong precision while passing stringent EMI /EMC certification tests. This session will address these systems and their challenges by explaining each configuration, and explaining example designs
Concepts of Switching Regulator EMI and Noise Mitigation
Before we dive into specific application-based examples of noise and EMI mitigation, let's start with the basics. What is noise? What is EMI? What is ripple? How are they measured? What are some common approaches to limiting their effects? This section discusses these topics with a more conceptual approach to serve as a primer for the rest of the series.
Resources:
EMI and Noise Mitigation Techniques in Practice
Now that we understand the sources of EMI and noise in switching regulators, and some of the common approaches to mitigating each, let's take a closer look at real-world examples of reducing their effects. In this section we will examine the impacts of various mitigation techniques to help you decide which approach makes the most sense in your design. Techniques covered in this discussion include external component placement, filter options and design, frequency manipulation via spread spectrum or dithering, snubbers, boot resistors, and more.
Resources:
Achieving low noise and high efficiency for noise-sensitive analog loads
Noise and EMI can be detrimental to sensitive analog signal chain circuitry. For this reason, many engineers automatically default to linear regulators. But, in doing so, they are essentially trading one problem (noise) for another (heat dissipation). In this section we will discuss what types of signal chain loads can be driven directly by a switching regulator to get low noise and EMI without sacrificing efficiency. We will also discuss when a linear regulator is absolutely needed to reach levels of noise not possible with a switcher.
Resources:
Low EMI and low noise DC/DC conversion in Automotive applications
Because of the potential havoc that interference can wreak in radio and safety critical systems, automotive electronics are subject to the most stringent EMI standards- the most common being CISPR25 Class-5. The materials below provide a discussion around the sources of EMI in an automotive environment and a comprehensive blueprint to understanding how to minimize it's effects.
Resources:
TAS5825M Innovation Features Overview
What are the audio amplifier requirements for wireless / AI speaker? How TAS5825M improve battery lifetime and audio quality?
This section provides the overview of TAS5825M innovation features.
TAS5825M Hybrid PWM Modulation to Improve Battery Efficiency
Compared with traditional PWM modulation, TAS5825M develops innovative Hybrid modulation, which dynamically maintains differential switching with several common duty options.
The benefits of Hybrid PWM modulation mainly includes:
- Higher efficiency for longer battery lifetime
- Good THD+N performance
- Ultra-low idle power dissipation and idle noise
TAS5825M Thermal Foldback, Inductor Free and Audio DSP Resource
This training section descripts some innovation features of TAS5825M, which includes:
- Real-time thermal foldback: maintain max safe output power for uninterrupted listening experience
- 122MHz DSP resource: 192kHz high definition audio processing or Smart Amp algorithm for better speaker protection
- Inductor less: state-of-the-art EMI reduction technology
Mastering the art of high voltage gate drivers
In this training series, we will touch the gate driver applications, fundamentals of low side gate driver, high- and low side gate driver and isolated gate driver. And we will surely go deep and help you understand the gate driver design considerations with TI reference design and the corresponding critical waveforms.