Hint: separate multiple terms with commas

E.g., 02/23/2018

E.g., 02/23/2018

Hint: separate multiple terms with commas

E.g., 02/23/2018

E.g., 02/23/2018

Sort by:

142 Results

KeyStone Multicore Navigator

Date:
November 1, 2010
This module provides an introduction to the architecture and functional components of the Multicore Navigator, which includes the Queue Manager Subsystem (QMSS) and Packet DMA (PKTDMA).

KeyStone Multicore Navigator: Queue Manager Subsystem (QMSS)

Date:
November 1, 2010
This module provides a detailed look at the functional elements of the QMSS and provides information on programming QMSS through the use of registers and low level drivers.

KeyStone Multicore Navigator: Packet DMA

Date:
November 1, 2010
This module provides a detailed look at the infrastructure and functional aspects of the PKTDMA and provides information on programming PKTDMA through the use of registers and low level drivers.

KeyStone Inter-Processor Communication (IPC)

Date:
December 1, 2012
This module provides an overview of the hardware and software that transports data and/or signals between threads of execution in KeyStone I C66x DSP multicore devices.

KeyStone External Interfaces (EMIF-A, UART, I2C, SPI, TSIP)

Date:
November 1, 2010
This module provides an overview of selected external interfaces on KeyStone devices including UART, I2C, SPI, TSIP, and EMIF-A.

KeyStone Serial Rapid IO (SRIO)

Date:
November 1, 2010
This module takes a look at the new features and enhancements of the SRIO on KeyStone devices.

KeyStone FFT Co-Processor (FFTC)

Date:
November 1, 2010
This module presents the architecture and features of the FFT co-processor.

KeyStone Turbo Decoder Co-Processor (TCP3D)

Date:
November 1, 2010
This module provides an overview of TCP3D including key features, modes, drivers, and configuration. Examples are provided.

KeyStone Turbo Encoder Co-Processor (TCP3E)

Date:
November 1, 2010
This module provides an overview of TCP3E including usage, initialization, and configuration. Examples are provided.

Multicore Software Development Kit (MCSDK) for KeyStone Devices

Date:
October 1, 2011
This module provides an overview of the multicore SoC software for KeyStone I C66x DSP devices. This module introduces the optimized software components that enable the rapid development of multicore applications and accelerate time to market using foundational software in the MCSDK. The MCSDK also enables developers to evaluate the hardware and software capabilities using the C66x evaluation module.

KeyStone Bootloader Overview

Date:
November 1, 2010
This module provides an introduction to the C66x bootloader including configuration, device startup, and run-time modes.

KeyStone Power Management

Date:
June 1, 2016
This module provides an overview of the C66x power domain topology, power-saving features, power and clocking domains, power states, and Smart Reflex.

KeyStone ARM & DSP Multicore Device Training Series

This training series provides an in-depth look at KeyStone multicore SoC devices.

Save Energy with LED Lighting and Intelligent Sensing

Date:
March 18, 2015

Duration:
43:58
Main benefit of LEDs is that you can save energy by dimming the light. So what about an intelligent light which is aware of its environment and communicates to other lights on the need for illumination? From simple temperature measurement, ambient light and occupancy sensing using TI MCUs and DSPs to wired and wireless communication protocols TI’s software and hardware solutions help to design Intelligent Lighting.

C Compiler Tips & Tricks

Date:
March 18, 2015

Duration:
58:29
This presentation is intended for those new to TI C/C++ compiler tools. It is a collection of tips and tricks beginners usually find useful. The information applies equally well to all TI compilers. Those with experience programming general-purpose processors will appreciate the tips on how things differ when programming for TI embedded processors.

TI-RTOS Overview

Date:
May 13, 2015

Duration:
32:14
This session provides an in-depth overview of TI-RTOS features and device support

Processor SDK Overview

Date:
September 24, 2015
This module provides an introduction to the Processor Software Development Kit (SDK), the next generation unified software platform for TI’s newest processor families. In addition to providing an overview of the benefits of a scalable Linux and TI-RTOS Processor SDK, this lesson takes a look at how SoC processor cores help determine the software used for application development, introduces the OS-based Processor SDK architectures, and shows how they complement the broader TI software development ecosystem.

Introduction to Processor SDK RTOS Part 1

Date:
October 8, 2015
This module is the first installment of a two-part overview of the Processor SDK from the TI-RTOS perspective. It introduces the functional elements that may be included in the installation for an SoC, and then looks at these elements in more detail: TI-RTOS kernel, Inter-Processor Communication (IPC), Network Developer's Kit (NDK), algorithm libraries, and diagnostic software.

Introduction to Processor SDK RTOS Part 2

Date:
October 8, 2015
This module is the second installment of a two-part overview of the Processor SDK from the TI-RTOS perspective. It examines the functional elements that may be included in the installation for an SoC: Low-level Drivers (LLD), Chip Support Library (CSL), OS Abstraction Layer (OSAL), board library, Secondary Boot Loader (SBL), and board diagnostics.

Application Development Using Processor SDK RTOS

Date:
October 8, 2015
This presentation provides a detailed overview of the application development process using the Processor SDK RTOS release. It walks through each step of the a typical development flow, including setup of the evaluation module (EVM), getting started with the EVM, running out-of-box examples, developing application code, porting applications to custom hardware, and customization of application software.
142 Results