Hint: separate multiple terms with commas

E.g., 01/21/2020

E.g., 01/21/2020

Hint: separate multiple terms with commas

E.g., 01/21/2020

E.g., 01/21/2020

Sort by:

174 Results

Type-C PD 於工業電腦與電子銷售系統的應用

課程說明 USB 的演進,並說明了 Type C 的通訊協定、電源傳輸協定,最後介紹了不同使用情境下 TI 的相關應用晶片。
Factory automation

Isolation in Industrial Systems

In 2019 more than 2.5 million industrial robots will be in operation worldwide, according to a forecast of the international federation of robotics. An industrial robot typically consists out of a control cabinet, a robot arm and a Human Machine Interface (HMI) Panel. To guarantee safe operation of the complete robot system, the different robot components and its interfaces need to be isolated to each other.

Factory automation

Isolated Power Supplies for PLC I/O Modules

The training starts with an overview of an analog input module. Typical components and their voltage supply levels are shown. Next, possible power topologies like push-pull, flyback or flybuck with their advantages and disadvantages are discussed.

Factory automation

How to add Industrial Ethernet to Computer Numeric Control (CNC) Router Machine

CNC routers use step and direction signals to control each stepper motors. In addition motor information (position, temperature, fault) gets transferred from stepper motors back to control unit. This must be done in star topology and a mix of proprietary interfaces. Simple open real-time Ethernet (SORTE) enables 4 µs cycle time on industrial Ethernet and replaces step/direction signal and motor feedback info into a single Ethernet cable that is also wired in line topology.

Factory automation

Learn Different Solutions to Design a Field Transmitter Ultrasonic AFE

A common method to measure process parameters in plants is based on sound waves. This method is used in: level, flow and displacement field transmitters. It works based on measuring the time of flight (ToF) between when the pulse, generated by a piezo electric crystal, is sent and received back by the piezo. 

Factory automation

Designing a Multi-Channel 4-20mA Analog Input Module

This training helps to understand relevant parameter of a 4-20mA analog input module, such as surge protection, handling miss-wiring, broken wire detection, isolation or protection of the module against over-current at power and signal inputs.

Factory automation

Design, Protection, and Technologies for Analog Outputs

Analog outputs in industrial automation come in a variety of configurations that each must deliver strong precision while passing stringent EMI /EMC certification tests.  This session will address these systems and their challenges by explaining each configuration, and explaining example designs

TI-RSLK

TI-RSLK Module 1 Running code on the LaunchPad using CCS

The purpose of this module is to learn software development methodology and understand how to set up an Integrated Development Environment (IDE), to then import and export Code Composer Studio (CCS) projects, as well as critical debugging information to understand the memory usage and performance of the software on the processor.

TI-RSLK

TI-RSLK Module 2 – Voltage, current, and power

The purpose of this course is to review basic electronic components and the electrical properties needed to interface sensors and actuators to a microcontroller. You will learn how to measure reactance of a capacitor and use your project to measure current and voltage. The electrical properties of the capacitor will help you design circuits that “filter” or remove noise from your robot.

TI-RSLK

TI-RSLK Module 3 – ARM Cortex M

This module serves as a brief introduction to the ARM Cortex-M microcontroller, assembly programming language and some debugging techniques. Understanding how the processor works is essential for the design of embedded systems, such as the one used in your robot.  

TI-RSLK

TI-RSLK Module 4 – Software Design using MSP432

This module is an introduction to C, a general-purpose programming language, in addition to the concepts of compiling and debugging using the MSP432 and TI Code Composer Studio™.  Debugging skills are a valuable tool when developing complex systems involved with robotics.

TI-RSLK

TI-RSLK Module 5 – Battery and voltage regulation

The purpose of this module is to learn how to power your robot. To run the robot (motor and other systems) you will need batteries and a regulator to provide constant voltage.  Understanding the relationship between voltage current and power is an essential component of robot system design.

TI-RSLK

TI-RSLK Module 6 – GPIO

In this module, you will interface a line sensor (infra-red sensor) to the microcontroller and learn how to write software to initialize GPIO pins.  The line sensor is a simple and accurate sensor for solving robotic challenges.

TI-RSLK

TI-RSLK Module 7 – Finite state machines

This module will demonstrate how to use finite state machines as a central controller for the system.

TI-RSLK

TI-RSLK Module 8 – Interfacing input and output

The purpose of this module is to develop interface switches and an LED so the robot can effectively detect wall collisions. Many sensors and actuators deploy LEDs, so understanding how they operate will be important to building your robot.

TI-RSLK

TI-RSLK Module 9 – SysTick timer

In this module, you will learn the fundamentals of SysTick timers and pulse width modulators (PWM), including how to measure pulse times and period with a logic analyzer and amplitude with an oscilloscope. It is important to understand the concept of PWM as we will use it to adjust power to the motors.

TI-RSLK

TI-RSLK Module 10 – Debugging real-time systems

This module provides an intro to how flash memory operates, including debugging techniques for real-time systems and how to generate periodic interrupts using SysTick. Minimally intrusive debugging is essential for real-time systems to evaluate performance while the system runs in real-life situations.

TI-RSLK

TI-RSLK Module 11 – Liquid Crystal Display

This module will show you how to display characters and provide real-time debugging on an LCD screen. An LCD on your robot provides a convenient way to observe what it is thinking.

TI-RSLK

TI-RSLK Module 12 – DC motors

The purpose of this lab is to interface the motors to the TI LaunchPad to make the robot move. Understanding how duty cycle, voltage and current combine to affect speed is required when building your robot.

174 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki