Hint: separate multiple terms with commas

E.g., 12/11/2019

E.g., 12/11/2019

Hint: separate multiple terms with commas

E.g., 12/11/2019

E.g., 12/11/2019

Sort by:

885 Results

Implementing isolated shunt sensors using metrology AFEs and external isolators

In this section, the isolated metrology AFE architecture will be discussed.   The software and hardware design considerations for this architecture will be discussed.  In addition, the TIDA-01550 isolated metrology AFE reference design will also be discussed.

Implementing isolated shunt sensors using isolated delta sigma modulators and digital filters

In this section, the isolated modulator architecture will be discussed.  The software and hardware design considerations for this architecture will be discussed.  In addition, various isolated modulator designs will also be discussed and compared.

Comparisons between isolated shunt sensing architectures

Both isolated modulator and isolated metrology AFE architectures have their advantages with respect to each other.  Depending on system requirements, one architecture may be more feasible than the other.  This section compares the two isolated shunt sensing architectures and discusses which architecture is best for different system requirements.

Summary

In this section, a summary of the entire “Polyphase Current Measurement with Isolated Shunt Sensors” training module would be covered.  Links will be provided for the reference designs that were discussed during this training series.

Smart Factory

Find below the block diagrams related to the Smart Factory demo

Smart Building

Find below the block diagrams related to the Smart Building demo

Powering

Find below the block diagrams related to the Powering demos

Sensing

Find below the block diagrams related to the Sensing demos

Controlling

Find below the block diagrams related to the Controlling demos

Connecting

Find below the block diagrams related to the Connecting demos
South Asia Industrial Webinar

Design considerations for USB type-C power delivery

The presentation addresses the design consideration of USB Type-C power delivery. USB Type-C is the new trend of Industrial, automotive and personal electronics devices. In the training, audience will be able to learn more about USB Type-C power delivery (PD) requirement and understand architecture of USB Type-C PD, AC/DC power source.

South Asia Industrial Webinar

Environmental sensor for building automation design

Building automation system is a communication network infrastructure that manages the building service. This training will introduce the environmental sensor black diagram, key reference design and the solution for IC temperature sensor, power saving analog temperature sensor, digital temperature sensor … etc.

South Asia Industrial Webinar

SAR ADC Design

Targeting the Test and Measurement application, this section includes many topics relevant to designing with SAR ADC devices.

South Asia Industrial Webinar

Introduce high power DC/DC conversion design: comparison of PSFB and FB-LLC

The “conventional wisdom” is that the Phase Shifted Full Bridge (PSFB) topology is the best choice for high power DC/DC converter applications. However, the “conventional wisdom” has been challenged by the users who are choosing the Full Bridge LLC (FB-LLC) topology for applications where we would normally suggest the PSFB topology. The speaker provides a clear comparison between the two typologies and tries to indicate which is best in a given application.
South Asia Industrial Webinar

Overview of commonly-used interface for industrial application

The training provides a very comprehensive introduction of the commonly-used interfaces including RS-485, RS-422, ProfiBus, RS-232, IO-Link, CAN and LIN. These interfaces are used in the application of Factory Automation and some other industrial applications. For the engineer who needs to deal with interface system design, this is a very useful training.

Topologies

View a broad curriculum of training for designing with various power supply topologies, as well as step by step instructions to build complete power topology reference designs.

Solving Design Challenges

Get tips, tricks and techniques to solve common power supply design challenges with power experts.

Current sensor and metrology architecture options

This section compares two types of current sensors used in electricity meters: current transformers and shunts.  In addition, it discusses three different architectures for sensing the voltage and current samples used to calculate the metrology parameters.  These architectures include a SoC-based architecture, AFE-based architecture, and ADC-based architecture.

Introduction to TIDA-010037 reference design

This section provides an overview of the TIDA-010037 reference design, which uses the ADS131M04 delta sigma standalone ADC for sensing the voltage and current necessary to calculate metrology parameters.  The TIDA-010037 design targets Class 0.1 split-phase current transformer meters.
885 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki