Hint: separate multiple terms with commas

E.g., 06/01/2020

E.g., 06/01/2020

Hint: separate multiple terms with commas

E.g., 06/01/2020

E.g., 06/01/2020

Sort by:

993 Results

Sensing

Find below the block diagrams related to the Sensing demos

Controlling

Find below the block diagrams related to the Controlling demos

Connecting

Find below the block diagrams related to the Connecting demos
South Asia Industrial Webinar

Design considerations for USB type-C power delivery

The presentation addresses the design consideration of USB Type-C power delivery. USB Type-C is the new trend of Industrial, automotive and personal electronics devices. In the training, audience will be able to learn more about USB Type-C power delivery (PD) requirement and understand architecture of USB Type-C PD, AC/DC power source.

South Asia Industrial Webinar

Environmental sensor for building automation design

Building automation system is a communication network infrastructure that manages the building service. This training will introduce the environmental sensor black diagram, key reference design and the solution for IC temperature sensor, power saving analog temperature sensor, digital temperature sensor … etc.

South Asia Industrial Webinar

SAR ADC Design

Targeting the Test and Measurement application, this section includes many topics relevant to designing with SAR ADC devices.

South Asia Industrial Webinar

Introduce high power DC/DC conversion design: comparison of PSFB and FB-LLC

The “conventional wisdom” is that the Phase Shifted Full Bridge (PSFB) topology is the best choice for high power DC/DC converter applications. However, the “conventional wisdom” has been challenged by the users who are choosing the Full Bridge LLC (FB-LLC) topology for applications where we would normally suggest the PSFB topology. The speaker provides a clear comparison between the two typologies and tries to indicate which is best in a given application.
South Asia Industrial Webinar

Overview of commonly-used interface for industrial application

The training provides a very comprehensive introduction of the commonly-used interfaces including RS-485, RS-422, ProfiBus, RS-232, IO-Link, CAN and LIN. These interfaces are used in the application of Factory Automation and some other industrial applications. For the engineer who needs to deal with interface system design, this is a very useful training.

Current sensor and metrology architecture options

This section compares two types of current sensors used in electricity meters: current transformers and shunts.  In addition, it discusses three different architectures for sensing the voltage and current samples used to calculate the metrology parameters.  These architectures include a SoC-based architecture, AFE-based architecture, and ADC-based architecture.

Introduction to TIDA-010037 reference design

This section provides an overview of the TIDA-010037 reference design, which uses the ADS131M04 delta sigma standalone ADC for sensing the voltage and current necessary to calculate metrology parameters.  The TIDA-010037 design targets Class 0.1 split-phase current transformer meters.

TIDA-010037 hardware design

This section provides an overview of the hardware used in the TIDA-010037 design, which includes information on the eFuse circuit used to create a current limited rail for connection to an external communication module.  In addition, this section discusses the circuits used to translate the Mains voltage and current to the voltage waveform sensed by the ADS131M04.

Designing software for split-phase electricity meters that use standalone ADCs

This section covers the initialization code and algorithms that can be used to calculate metrology parameters in a split-phase system using the sensed voltage and current samples

Calibration and metrology accuracy results

This section discusses the procedure used to calibrate the TIDA-010037 design and the results obtained with this design.

Summary

In this section, a summary of the entire “How to design high-accuracy CT-based split-phase electricity meters using standalone metrology ADCs” training module would be covered.  Links will be provided for the reference designs that were discussed during this training series.

Current sensor and metrology architecture options

This section compares two types of current sensors used in electricity meters: current transformers and shunts.  In addition, it discusses three different architectures for sensing the voltage and current samples used to calculate the metrology parameters.  These architectures include a SoC-based architecture, AFE-based architecture, and ADC-based architecture.

Introduction to TIDA-010036 reference design

This section provide an overview of the TIDA-010036 reference design, which uses the ADS131M04 delta sigma standalone ADC for sensing the voltage and current necessary to calculate metrology parameters.  The TIDA-010036 design targets Class 0.5 single-phase two-wire meters with shunt current sensors and has a compact, magnetically immune cap-drop power supply to power the design from AC mains.

TIDA-010036 hardware design

This section provides an overview of the hardware used in the TIDA-010036 design, which includes the circuits used to translate the Mains voltage and current to the voltage waveform sensed by the ADS131M04.  In addition, it covers the TPS7A78-based cap-drop power supply used in this design.

Designing software for 1-phase electricity meters that use standalone ADCs

This section covers the initialization code and algorithms that can be used to calculate metrology parameters in a single-phase system using the sensed voltage and current samples.

ADS131M04 current detection mode for detecting neutral removal tampering

This section discusses current detection mode, which is a special low-power mode of the ADS131M04 standalone ADC, that can detect the presence of current when someone has tampered with a meter by removing its neutral connection.

Calibration and metrology accuracy results

This section discusses the procedure used to calibrate the TIDA-010037 design and the results obtained with this design.
993 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki