Hint: separate multiple terms with commas

E.g., 01/27/2020

E.g., 01/27/2020

Hint: separate multiple terms with commas

E.g., 01/27/2020

E.g., 01/27/2020

Sort by:

1085 Results

PSE Basics

See how things have changed for PSEs with the migration from .at to the new .bt standard. If you’re ready to start evaluating  whether our power sourcing equipment (PSE) controller is the right solution for your application, watch the below trainings to learn how to quickly configure or work with non-standard PD types.

PD Basics

Several features have either evolved or been added as an essential PoE capability in 802.3bt.  Learn why Autoclass is in high-demand, how our PD’s respond in power demotion events, and how to design your PD systems with hitless failover in mind.

Topology Introduction

Just getting started with LED or need a refresher on what tradeoffs to anticipate with different topologies? The below video provides a quick and easy-to-understand overview of five topologies.

Dimming Algorithms

This segment of the LED drivers basics series provide an overview of the basic relationship between LED current and light output, as well as the benefits and limitations of analog and PWM dimming methodologies. These videos are appropriate for engineers of all experience levels, serving as basic training for new LED driver design engineers or a memory refresh for more experienced designers.

Automotive LED Drivers

Reliability and efficiency are of the utmost importance in many automotive lighting systems. Get pointers on how to avoid or overcome common auto challenges in the follow videos.

RGB LED Drivers

RGB LED drivers are becoming more popular choices for applications like audio and voice recognition systems, or Human-Machine Interfaces where LED color and patterns are critical elements of the user-interface. Each of the first five videos quickly explains critical concepts to RGB LEDs, while the last video discusses a unique RGB LED functionality from TI that enables the LED driver to operate autonomously from your MCU. 

using the fusion GUI to configure a sequencer

Getting Started

This section explains how to connect the EVMs and download, install, and launch the Fusion Digital Power Designer.
using the fusion GUI to configure a sequencer

Using the Fusion Digital Power Designer

The Fusion Digital Power Designer is packed with features. Explore below to learn how to use them all.

Battery chargers

Watch recorded sessions from battery chargers track. For your convenience some of the sessions were split into smaller sessions. 

Battery gauges

Watch recorded sessions from battery gauges track. For your convenience some of the sessions were split into smaller sessions. 

Battery monitoring and protection

Watch recorded sessions from battery monitoring and protection track. For your convenience some of the sessions were split into smaller sessions. 
South Asia Industrial Webinar

Design considerations for USB type-C power delivery

The presentation addresses the design consideration of USB Type-C power delivery. USB Type-C is the new trend of Industrial, automotive and personal electronics devices. In the training, audience will be able to learn more about USB Type-C power delivery (PD) requirement and understand architecture of USB Type-C PD, AC/DC power source.

South Asia Industrial Webinar

Introduce high power DC/DC conversion design: comparison of PSFB and FB-LLC

The “conventional wisdom” is that the Phase Shifted Full Bridge (PSFB) topology is the best choice for high power DC/DC converter applications. However, the “conventional wisdom” has been challenged by the users who are choosing the Full Bridge LLC (FB-LLC) topology for applications where we would normally suggest the PSFB topology. The speaker provides a clear comparison between the two typologies and tries to indicate which is best in a given application.

Topologies

View a broad curriculum of training for designing with various power supply topologies, as well as step by step instructions to build complete power topology reference designs.

Solving Design Challenges

Get tips, tricks and techniques to solve common power supply design challenges with power experts.

Introduction to Power over Ethernet (PoE)

If you are brand new to PoE, we recommend watching all four videos at your own pace for a complete overview. If you’re more experienced with the technology and just need a refresher on various concepts, jump right into the topic that meets your needs. Or consider watching our more advanced series below on all things related to the IEEE 802.3bt design.

IEEE 802.3bt: Getting started with the new standard

The new IEEE 802.3bt standard has introduced the capability for designers to utilize PoE for high-power applications (up to 90W at source and 71.3 at input). The below videos provide insights into whether the .bt standard is right for you, but if you’re already evaluating or compliant to .bt, we’ve also shared resources to help you navigate working with non-standard PD types, response to power demotion events and more.

1085 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki