Hint: separate multiple terms with commas

E.g., 09/15/2019

E.g., 09/15/2019

Hint: separate multiple terms with commas

E.g., 09/15/2019

E.g., 09/15/2019

Sort by:

205 Results

SimpleLink™ Academy - TI Drivers | Configuring TI Drivers

When: March 9, 2017
This workshop will dive into the details on how to configure TI Drivers for all SimpleLink Devices. We'll use these different devices in this workshop but the concepts are the same for all TI Drivers on all SimpleLink devices.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - TI Drivers | Configuring TI Drivers

When: March 9, 2017
This workshop will dive into the details on how to configure TI Drivers for all SimpleLink Devices. We'll use these different devices in this workshop but the concepts are the same for all TI Drivers on all SimpleLink devices.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - Proprietary RF | Wireless Sensor Network example

When: March 7, 2017
This training will walk you through setting up the Wireless Sensor Network (WSN) example with the SimpleLink™ CC13xx device. When you have completed the training you will have a WSN consisting of a concentrator displaying data received from one or more sensor nodes. The nodes will be truly ultra low power and only wake up to send data if the measured ADC value (capacitive coupling on certain pins) changes by a certain threshold. This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible.   

SimpleLink™ Academy - Proprietary RF | Linux Gateway Project Zero

When: March 13, 2017
The TI 15.4-Stack Linux SDK example applications helps developers create ultra-low power, very long-range, star-topology network solutions. The TI 15.4-Stack Linux SDK includes the Collector and Gateway Example Applications (in addition to others; See the TI 15.4-Stack Embedded Developer’s Guide for more details). The Linux Collector Example Application interfaces over UART with a CC13x0 LaunchPad™, which acts as a MAC CoProcessor (CoP). The Collector Example Application implements a full-function device which performs the functions of a network PAN coordinator (starting a network and permitting devices to join this network) and also provides an interface for monitoring and collecting sensor data from one or more sensor devices. In addition, the Collector Gateway Example Application provides a socket server interface to the Linux Gateway Application. This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible.

SimpleLink™ Academy - Proprietary RF | EasyLink Network Processor example

When: March 7, 2017
This training will walk you through setting up the Easy Link Network Processor example, as well as using SmartRF Studio for RF evaluation. When you have completed the training you will be able to set up the TI-RTOS EasyLink AT command Network Processor example to run on supported hardware, e.g. the CC1310/CC1350 LaunchPad. This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - Proprietary RF | Basic RX and TX

When: March 7, 2017
The purpose of this exercise is to familiarize the users with the RF driver running on the SimpleLink™ CC13x0 device. Users will also use Code Composer Studio and SmartRF™ Studio, and will learn how to import and modify existing RX & TX example applications. Users will use 2 CC13x0 LaunchPad™ kits to send/receive data between them. This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - POSIX Project Zero

When: March 9, 2017
POSIX (Portable Operating System Interface) is an IEEE industry API standard for OS compatibility. The SimpleLink™ software development kits (SDKs) has both TI-RTOS and FreeRTOS support, however it also offers POSIX support on top of either of these RTOS's. This allows applications to be independent of the underlying RTOS. This workshop provides a simple introduction to using POSIX with the SimpleLink SDK. You will use TI Resource Explorer, the SimpleLink SDK, and CCS Cloud to modify a project and run it on a SimpleLink LaunchPad™ Development Kit. The goal for this project is to familiarize you with some POSIX APIs and concepts typically used in multithreaded applications. This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible.     

SimpleLink™ Academy - POSIX Project Zero

When: March 9, 2017
POSIX (Portable Operating System Interface) is an IEEE industry API standard for OS compatibility. The SimpleLink™ software development kits (SDKs) has both TI-RTOS and FreeRTOS support, however it also offers POSIX support on top of either of these RTOS's. This allows applications to be independent of the underlying RTOS.This workshop provides a simple introduction to using POSIX with the SimpleLink SDK. You will use TI Resource Explorer, the SimpleLink SDK, and CCS Cloud to modify a project and run it on a SimpleLink LaunchPad™ Development Kit. The goal for this project is to familiarize you with some POSIX APIs and concepts typically used in multithreaded applications.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - POSIX Project Zero

When: March 9, 2017
POSIX (Portable Operating System Interface) is an IEEE industry API standard for OS compatibility. The SimpleLink™ software development kits (SDKs) has both TI-RTOS and FreeRTOS support, however it also offers POSIX support on top of either of these RTOS's. This allows applications to be independent of the underlying RTOS.This workshop provides a simple introduction to using POSIX with the SimpleLink SDK. You will use TI Resource Explorer, the SimpleLink SDK, and CCS Cloud to modify a project and run it on a SimpleLink LaunchPad™ Development Kit. The goal for this project is to familiarize you with some POSIX APIs and concepts typically used in multithreaded applications.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - FreeRTOS | Project Zero

When: March 9, 2017
The SimpleLink™ MSP432™ and Wi-Fi® CC3220 software development kits (SDKs) include the ability to use FreeRTOS™ (as well as the TI-RTOS). This workshop will explain what this really means. Here's what we'll learn: How TI Drivers work with FreeRTOSPOSIX support with FreeRTOSUnderstand parts of FreeRTOS kernel projects This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - FreeRTOS | Project Zero

When: March 9, 2017
The SimpleLink™ MSP432™ and Wi-Fi® CC3220 software development kits (SDKs) include the ability to use FreeRTOS™ (as well as the TI-RTOS). This workshop will explain what this really means.Here's what we'll learn:How TI Drivers work with FreeRTOSPOSIX support with FreeRTOSUnderstand parts of FreeRTOS kernel projectsThis training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - Bluetooth LE | Custom Profile

When: March 9, 2017
Explanation of the GATT and ATT protocols that Bluetooth Low Energy data exchange is based on, a walk-through of how to implement a custom Bluetooth service using the APIs provided in the TI BLE SDK, and a basic code generator for custom servicesThis training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - Bluetooth LE | Bluetooth SDK Plugin

When: March 7, 2017
The SimpleLink™ MSP432™ SDK Bluetooth Plugin is made as a complimentary software package that adds full BLE capabilities to your SimpleLink MSP432 SDK projects. This training/exercise session is meant to provide a basic introduction of the "SDK Plugin" concept as well as give to users a quick hands-on experience using the SimpleLink MSP432 SDK Bluetooth Plugin. This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 

SimpleLink™ Academy - Bluetooth LE | Bluetooth Low Energy + Sensors BoosterPack

When: March 9, 2017
Learn how to port between devices in the SimpleLink family to read temperature data on the Simplelink CC2640R2 Wireless MCU. Enhance Project Zero by adding the ability to read and send temperature data over BLE.This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible.

SimpleLink™ Academy - Bluetooth LE | Bluetooth Developer Studio

When: March 9, 2017
Learn how to use the Bluetooth Developer Studio GUI by Bluetooth SIG and the TI Code Generator plugin to accelerate the development of your own custom services This training is delivered as part of SimpleLink™ Academy in TI Resource Explorer, a collection of curated training modules developed by TI subject matter experts to help developers get up and running as quickly as possible. 
simplelink academy, TI simplelink academy training, simplelink training, software training, sdk training

Simplelink™ Academy

SimpleLink Academy provides a comprehensive and interactive learning experience for the SimpleLink portfolio of devices covering all phases of development from basic examples to more advanced optimization techniques that help fine tune your design. SimpleLink Academy is housed on our TI Resource Explorer and lives within each SDK.

Watch the overview videos to find out more, or click on your technology and software development kit to be redirected to the SimpleLink Academy modules. 

SimpleLink Wi-Fi CC3220 and CC3120 Product Overview

Date:
May 4, 2017

Duration:
01:15:54
The CC3220 wireless MCU and CC3120 Network Processor are the second generation of TI’s Internet-on-a-chip™ family of solutions.
SimpleLink Sensor to Cloud Demo

SimpleLink Sensor to Cloud Building and Factory Automation Demo

Date:
December 21, 2017

Duration:
06:11
Live Demo featuring TI's SimpleLink MCUs streaming sensor data to the cloud through an Intelligent factory automation and a smart home control system
SimpleLink MSP432P4111 out of box experience

SimpleLink MSP432P411 Out of Box Experience

Date:
August 7, 2018

Duration:
06:38
Getting started with the SimpleLink MSP432P4111™ LaunchPad and GUI.

SimpleLink MSP432E4 ProfiNET & Wireless Motor Condition Gateway Solution

Date:
November 29, 2017

Duration:
02:28
This video will demonstrate the SimpleLink MSP432E4 Ethernet MCU running the ProfiNET Conformance Class-A
205 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki