Hint: separate multiple terms with commas

E.g., 10/16/2019

E.g., 10/16/2019

Hint: separate multiple terms with commas

E.g., 10/16/2019

E.g., 10/16/2019

Sort by:

1198 Results

DS90UB953/954 System Design & Operation: Sensor-953 Link Design

This is the Sensor and 953 Link Design section in DS90UB953/954 System Design & Operation video series. This video discusses how to use the sensor-953 link, as well as, the specific settings that are used with this link.

DS90UB953/954 System Design & Operation: 954-ISP/SoC Link Design

This section discusses what frame synchronization (FrameSync) is and how to configure in on the 953 and 954 and how CSI2 data is transferred across the link from the 954 to the ISP/SoC

Specifically, this section discusses: Frame Synchronization (FrameSync), Controlling 953 GPIOs locally and remotely via I2C, Unsynchronized and synchronized sensors, Internal and External Frame Sync, Port Forwarding, Accessing Indirect Registers, and Pattern Generation on 953 & 954

DS90UB953/954 System Design & Operation: Hardware Design

This section discusses how design a 953/954 using Power over Coax (PoC), and various hardware checks and concepts that need to be considered when analyzing a 953/954 system.

Specifically, this section discusses: Power Over Coax (PoC), AC Coupling Capacitors, PoC Inductors, Typical PoC Schematic, Critical Signal Routing, I2C Pullups, Loop Filter Capacitors on 953, Insertion Loss, Return Loss, and Time Domain Reflection (TDR) measurements.

Factory automation

Isolation in Industrial Systems

In 2019 more than 2.5 million industrial robots will be in operation worldwide, according to a forecast of the international federation of robotics. An industrial robot typically consists out of a control cabinet, a robot arm and a Human Machine Interface (HMI) Panel. To guarantee safe operation of the complete robot system, the different robot components and its interfaces need to be isolated to each other.

Factory automation

Isolated Power Supplies for PLC I/O Modules

The training starts with an overview of an analog input module. Typical components and their voltage supply levels are shown. Next, possible power topologies like push-pull, flyback or flybuck with their advantages and disadvantages are discussed.

Factory automation

How to add Industrial Ethernet to Computer Numeric Control (CNC) Router Machine

CNC routers use step and direction signals to control each stepper motors. In addition motor information (position, temperature, fault) gets transferred from stepper motors back to control unit. This must be done in star topology and a mix of proprietary interfaces. Simple open real-time Ethernet (SORTE) enables 4 µs cycle time on industrial Ethernet and replaces step/direction signal and motor feedback info into a single Ethernet cable that is also wired in line topology.

Factory automation

Learn Different Solutions to Design a Field Transmitter Ultrasonic AFE

A common method to measure process parameters in plants is based on sound waves. This method is used in: level, flow and displacement field transmitters. It works based on measuring the time of flight (ToF) between when the pulse, generated by a piezo electric crystal, is sent and received back by the piezo. 

Factory automation

Designing a Multi-Channel 4-20mA Analog Input Module

This training helps to understand relevant parameter of a 4-20mA analog input module, such as surge protection, handling miss-wiring, broken wire detection, isolation or protection of the module against over-current at power and signal inputs.

Factory automation

Design, Protection, and Technologies for Analog Outputs

Analog outputs in industrial automation come in a variety of configurations that each must deliver strong precision while passing stringent EMI /EMC certification tests.  This session will address these systems and their challenges by explaining each configuration, and explaining example designs

Low EMI and Noise performance with DC/DC switching regulators

Concepts of Switching Regulator EMI and Noise Mitigation

Before we dive into specific application-based examples of noise and EMI mitigation, let's start with the basics. What is noise? What is EMI? What is ripple? How are they measured? What are some common approaches to limiting their effects? This section discusses these topics with a more conceptual approach to serve as a primer for the rest of the series. 

Resources:

Low EMI and Noise performance with DC/DC switching regulators

EMI and Noise Mitigation Techniques in Practice

Now that we understand the sources of EMI and noise in switching regulators, and some of the common approaches to mitigating each, let's take a closer look at real-world examples of reducing their effects. In this section we will examine the impacts of various mitigation techniques to help you decide which approach makes the most sense in your design. Techniques covered in this discussion include external component placement, filter options and design, frequency manipulation via spread spectrum or dithering, snubbers, boot resistors, and more.

Resources:

Low EMI and Noise performance with DC/DC switching regulators

Achieving low noise and high efficiency for noise-sensitive analog loads

Noise and EMI can be detrimental to sensitive analog signal chain circuitry. For this reason, many engineers automatically default to linear regulators. But, in doing so, they are essentially trading one problem (noise) for another (heat dissipation). In this section we will discuss what types of signal chain loads can be driven directly by a switching regulator to get low noise and EMI without sacrificing efficiency. We will also discuss when a linear regulator is absolutely needed to reach levels of noise not possible with a switcher.

Resources:

Low EMI and Noise performance with DC/DC switching regulators

Low EMI and low noise DC/DC conversion in Automotive applications

Because of the potential havoc that interference can wreak in radio and safety critical systems, automotive electronics are subject to the most stringent EMI standards- the most common being CISPR25 Class-5. The materials below provide a discussion around the sources of EMI in an automotive environment and a comprehensive blueprint to understanding how to minimize it's effects.

Resources:

Power factor correction (PFC) basics

Learn what power factor correction (PFC) is, the basics of power factor measurement and why PFC is needed. Also learn about EN6100-3-2 and Energy Star standards for power supplies.

Power factor correction (PFC) classification and control laws

Learn the difference between different PFC classifications and the advantages and disadvantages of peak current mode control, average current mode control and hysteresis current mode control.

Power factor correction (PFC) topology comparison

Learn about the advantages and disadvantages of classic boost PFC, dual boost bridge-less PFC, totem-pole bridge-less PFC and interleaved boost PFC. Also learn about the main power loss components in typical PFC circuits resulting in bridge low, choke loss, boost diode loss and switch loss.

How to design an efficient power factor correction (PFC) circuit

Learn the calculations and considerations required to design an efficient PFC choke inductor. Also learn how to further optimize efficiency and achieve a stable system. Finally, discover PCB layout considerations for power stage and control stage.

Power factor correction (PFC) design example

Learn about the design methodology and test results from the 230 V, 3.5 kW power factor correction (PFC) reference design.

Introduction to FPD-Link SerDes

These introduction videos describe the evolution of FPD-Link product families, and introduction to FPD-Link III SerDes for use in Infotainment and ADAS applications.

1198 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki