Hint: separate multiple terms with commas

E.g., 02/19/2020

E.g., 02/19/2020

Hint: separate multiple terms with commas

E.g., 02/19/2020

E.g., 02/19/2020

Sort by:

208 Results
using the fusion GUI to configure a sequencer

How to use the Fusion Digital Power Designer with UCD90x Sequencers

The Fusion Digital Power Designer is a PMBus based guided user interface (GUI) that allows users to configure TI’s family of UCD90X digital sequencers. This training series walks designers through how to work with the GUI to configure their UCD90X devices, and then manage and monitor their system accordingly.
using the fusion GUI to configure a sequencer

Getting Started

This section explains how to connect the EVMs and download, install, and launch the Fusion Digital Power Designer.
using the fusion GUI to configure a sequencer

Using the Fusion Digital Power Designer

The Fusion Digital Power Designer is packed with features. Explore below to learn how to use them all.

Exploring the Value of Power Modules

DC/DC Power Modules are best known for being compact, highly-integrated power supply design options. This training series examines some of the lesser-known advantages of TI power modules:

  1. How do Power Modules simplify power supply design?
  2. Inductor withstand voltage
  3. High temperature storage testing

MOSFET 101

Learn the basic tips and tricks to select and design with a MOSFET to get to market faster.

WEBENCH Power Designer: Step by Step

WEBENCH Power Designer makes end-to-end power supply design fast and intuitive. This video series describes each step of the WEBENCH process: Device selection, customization, simulation, and exporting designs to the next environment. 

Battery chargers

Watch recorded sessions from battery chargers track. For your convenience some of the sessions were split into smaller sessions. 

Battery gauges

Watch recorded sessions from battery gauges track. For your convenience some of the sessions were split into smaller sessions. 

Battery monitoring and protection

Watch recorded sessions from battery monitoring and protection track. For your convenience some of the sessions were split into smaller sessions. 

Reducing EMI via considerations external to the IC

For many engineers, layout for EMI mitigation is a black art. It may seem like the slightest adjustment could be the difference between passing or failing CISPR standards. Because of this, some power designers may shy away from using devices with switching elements as a guaranteed way to avoid the headache of reducing emissions. But this may be trading one problem for another, as switching devices generally have better efficiency and thermal performance.

Modules EMI

Reducing EMI through device selection

Efficiently addressing EMI starts at the device selection stage. On-silicon technologies like spread spectrum or unique packaging approaches like HotRod™ QFN can help reduce EMI before we even begin the discussion of component layout and filtering. 

Resources:

EMI: The Fundamentals

Before we dive into specific application-based examples of noise and EMI mitigation, let's start with the basics. What is EMI? How is this different from noise? What is ripple? How are they measured? What are some common approaches to limiting their effects? This section discusses these topics with a more conceptual approach to serve as a primer for the rest of the series. 

Resources:

Low EMI

Designing a Low EMI Power Supply

Mitigating EMI is seen by engineers as a black art. Choose the wrong feature set - or mess with the feng shui of the PCB layout too much - and the system may not pass stringent CISPR standards. 

This training series - along with all of the accompanying documentation - is an aggregation of reference materials showing how engineers an easier path to design an efficient power supply that meets EMI requirements.

Not All Regulators Are Created Equal

Explore several subtle nuances to significantly improve power supply performance. Examples include: the hidden advantages of synchronous regulators, a module that features the best attributes of a switcher AND an LDO, and tips to reduce system noise by manipulating output capacitor combinations.

Engineer It LDO Training Videos

These training videos will be used to better understand LDOs, and includes more information on designing the best ADC power supply, stabilizing an LDO, measuring LDO noise and power supply rejection ratio, sourcing 5-A or more with current sharing regulators, measuring thermal resistance between junction temperature and ambiance, and measuring the ADC power supply rejection. 

Type-C PD 於工業電腦與電子銷售系統的應用

課程說明 USB 的演進,並說明了 Type C 的通訊協定、電源傳輸協定,最後介紹了不同使用情境下 TI 的相關應用晶片。
South Asia Industrial Webinar

Design considerations for USB type-C power delivery

The presentation addresses the design consideration of USB Type-C power delivery. USB Type-C is the new trend of Industrial, automotive and personal electronics devices. In the training, audience will be able to learn more about USB Type-C power delivery (PD) requirement and understand architecture of USB Type-C PD, AC/DC power source.

South Asia Industrial Webinar

Introduce high power DC/DC conversion design: comparison of PSFB and FB-LLC

The “conventional wisdom” is that the Phase Shifted Full Bridge (PSFB) topology is the best choice for high power DC/DC converter applications. However, the “conventional wisdom” has been challenged by the users who are choosing the Full Bridge LLC (FB-LLC) topology for applications where we would normally suggest the PSFB topology. The speaker provides a clear comparison between the two typologies and tries to indicate which is best in a given application.

Topologies

View a broad curriculum of training for designing with various power supply topologies, as well as step by step instructions to build complete power topology reference designs.

Application-Specific EMI Considerations

Some systems simply require more attention than others when it comes to EMI. In this section, we will examine some of those specific end applications and provide some helpful hints to reach EMI targets with each.

Resources:

208 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki