Sort by:

25 Results
25 functions for 25 cents using TI’s MSP430 Value Line Sensing microcontrollers

25 Functions for 25 Cents Video Series

Simple functions such as timer replacement, input/output expanders, system reset controllers and stand-alone EEPROM are common on PCBs. Low-cost, ultra-low-power MSP430™ value line  microcontrollers (MCUs) offer cost savings when replacing digital and analog functions in a system. Watch this series to see how MSP430 MCUs can be used to enhance communication, pulse width modulation, systems and housekeeping, and timer functions in your next design.

66AK2Gx Processor Training Series

Similar to existing KeyStone-based SoC devices, the 66AK2Gx enables both the DSP and ARM cores to master all memory and peripherals in the system. This architecture facilitates maximum software flexibility where either DSP- or ARM-centric system designs can be achieved. 

This curriculum provides an in-depth look at the K2G Processors, Processor SDK-Linux and TI-RTOS, and the Programmable Realtime Unit (PRU).

Anti-tamper Techniques to Thwart Attacks on Smart Meters

Non-technical losses (“theft”) account for billions of dollars of revenue loss for utility providers around the world as individuals are able to hack meters to slow or stop the accumulation of energy usage statistics. This loss has driven increased requirements for enhancing the protection designed into new smart meters.  This training session will discuss different methods of attacking smart meters and how TI’s analog portfolio can be used to detect or even prevent these attacks. In one scenario magnets are used to saturate any transformers present in the system.

Battery and system monitoring for smart meters

Over the last few years, the industry has been moving from mechanical to fully electronic meters. We have seen more and more functionalities such as metrology with ultrasonic technology, leak detection with audio patterns, communication with low power and long range radio being added to smart meters. These new functionalities allow utilities to deliver new services such as condition-based maintenance and remote monitoring of meters, which lead to efficient management of the network and better customer experience.

Battery Powered Motor Drives: How to Design a High Performance Power Stage?

Modern battery powered motor drive applications such as power tools, drones, vacuum cleaners, eBikes, etc. show a clear trend towards permanent magnet synchronous motors (PMSM) and brushless DC motors (BLDC). The biggest challenge in designing the power stage for these applications is to meet form factor, efficiency, protection, peak current carrying capability and thermal performance. This training will explain how to do a system design to meet the design challenges  by proper selection of power FET and gate driver.

Create an Industrial 3D Machine Vision System using DLP® Technology

Create an Industrial 3D Machine Vision System using DLP® Technology

This DLP® training series helps users understand the most common 3D machine vision techniques.  The series includes the following key content:

Designing 6.6kW Bidirectional HEV/EV On-Board-Charger with SiC and Embedded Technologies

In this series of presentations, we go through the HEV/EV market status and history, OBC specifications, technology trend, topology selections and design considerations of an OBC system. Complete test results of a 6.6kW OBC reference design (Including AC-DC rectifier and isolated DC-DC converter) will be shown in the end of this paper to demonstrate the performance of our TIDesigns as well as TI SiC and embedded Technologies.

EtherCAT® Master on Sitara™ Processors Training Series

This training presents TI’s ready-to-use EtherCAT masters solutions for Sitara processors. EtherCAT master on Sitara runs on different operating systems, including TI-RTOS and RT Linux. It also runs on the EMAC interfaces (CPSW and PRU ICSS_EMAC) of any Sitara device, including AM57x, AM437x, and AM335x.

From Zero to Hero: Time-of-Flight Training (ToF) Series

From Zero to Hero: Time-of-Flight (ToF) Training Series

This training series will teach you about time-of-flight (ToF) technology and provide some tools and resources to help you prototype faster.

Getting started with the AFE74xx RF-sampling transceiver

Quickly evaluate the AFE7444 and/or AFE7422 RF-sampling transceiver with this series of how to videos.

How to design 1-phase shunt electricity meters using standalone metrology ADCs

As processing requirements for electricity meters gradually increase, it becomes increasingly difficult to find one device that meets both the processing requirements for adding advanced metrology features to smart meters while also accurately sensing metrology parameters, such as RMS voltage, RMS current and active power.  To deal with this design challenge, one option is to use a separate metrology microcontroller and a standalone ADC.

How to design high-accuracy CT-based split-phase electricity meters using standalone metrology ADCs

As processing requirements for electricity meters gradually increase, it becomes increasingly difficult to find one device that meets both the processing requirements for adding advanced metrology features to smart meters while also accurately sensing metrology parameters, such as RMS voltage, RMS current, and active power.  To deal with this design challenge, one option is to use a separate metrology microcontroller and a standalone ADC.

Layout, power loss, and packaging to address thermal concerns with integrated FET DC/DC converters

This training series dives into how to get the best thermal performance with TI’s latest buck converters. Special focus given to the HotRod package.

Mobile Smart TV training

Mobile Smart TV is a growing category that can extend the AV personal electronics category.  This training includes all the information you will want  to know about the mobile Smart TV category.  Introduction, value proposition, benefits, and design considerations of the mobile smart TV category are included in the training.  The last section, covers the benefits of DLP Pico technology for this application.

The MSP-EXP430FR2355 LaunchPad development kit training

MSP-EXP430FR2355 LaunchPad Development Kit Training

The MSP-EXP430FR2355 LaunchPad™ development kit is a member of the MSP430™ Value Line MCU family. The LaunchPad kit provides a quick evaluation and prototyping tool for the MSP430FR2355 microcontroller (MCU). This series provides an overview of the LaunchPad kit’s features and the out-of-box light sensing and smart analog combo GUI demos.
MSP-EXP430FR2433 – the MSP430FR2433 Microcontroller LaunchPad Development Kit

MSP-EXP430FR2433 LaunchPad Development Kit Training

The MSP-EXP430FR2433 LaunchPad™ development kit is a member of the MSP430™ Value Line Sensing MCU family. The LaunchPad kit provides a quick evaluation and prototyping tool for the MSP430FR2433 microcontroller (MCU). This series provides an overview of the LaunchPad kit’s features and the out-of-box temperature sensing demo.

MSP430 MCUs Smart Analog Combo training

Did you know that you can use a microcontroller to recognize many analog signal chain configurations? The MSP430 MCU portfolio has two device families, the MSP430FR2355 and MSP4302311, that have many configurable signal chain elements. Using this feature can help you save BOM costs and simplify board complexity.

RF Mesh Networking Offers System Performance and Interoperability

IPv6-based communications networks are becoming the standard choice in industrial markets such as smart meters and grid automation. These 6LoWPAN-based mesh networks address key concerns such as vendor interoperability, long-distance connectivity, security and reliability. This training will cover system- and software-level deep-dives on new RF 6LoWPAN mesh solutions, which implement open-source based 6LoWPAN mesh stacks on top of the frequency hopping based TI-15.4 stack.

Learn about multiplexers

TI Precision Labs - Multiplexers

TI Precision Labs is the electronics industry’s first comprehensive online classroom for analog engineers. The on-demand curriculum pairs theory and applied lab exercises to deepen the technical expertise of experienced engineers and accelerate the development of those early in their career. This free modular curriculum includes more than 40 hands-on training and lab videos, covering analog amplifier design considerations with online course work.

25 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki