Sort by:

76 Results

6LoWPAN RF mesh demo and summary

This session will show a 6LoWPAN mesh demo and then conclude our discussion with summary.

6LoWPAN-based Wireless Network Protocols

This section covers system-level deep dive on key wireless network protocols of 6LoWPAN, RPL, and CoAP for smart grid IoT. 

LC-sensing solution with TI FemtoFET and CC1350 Sensor Controller Engine

7-segment LCD control thru SW and GPIOs

This module covers the “Innovative 7-Segment LCD Control Using GPIO Pins and SW” section of the “Single-chip Smart Water meter with Dual-band RF link and InfraRed port” training series.

AC Analog Input Module Architecture (AIM)

The third part of the session provides details on the need to focus on AC analog input module and its use cases in different types of protection relays, Different types of current sensors and the use cases for these sensors including key advantages and dis-advantages. Explains AC analog input module architecture including block diagram showing the critical products and EERD with different subsystems identified showing different approaches for designing an AC AIM.

EV Charging (Pile) Stations Design Considerations

AC and DC Charging (Pile) Station Design Considerations

Gain a deep dive into common design consideration for a Level 1, 2 or 3 EV charging (pile) station and explore the service equipment block diagram for each.

ADS131M04 current detection mode for detecting neutral removal tampering

This section discusses current detection mode, which is a special low-power mode of the ADS131M04 standalone ADC, that can detect the presence of current when someone has tampered with a meter by removing its neutral connection.

Anti-tamper Techniques to Thwart Attacks on Smart Meters

Non-technical losses (“theft”) account for billions of dollars of revenue loss for utility providers around the world as individuals are able to hack meters to slow or stop the accumulation of energy usage statistics. This loss has driven increased requirements for enhancing the protection designed into new smart meters.  This training session will discuss different methods of attacking smart meters and how TI’s analog portfolio can be used to detect or even prevent these attacks. In one scenario magnets are used to saturate any transformers present in the system.

Battery and system monitoring for smart meters

Over the last few years, the industry has been moving from mechanical to fully electronic meters. We have seen more and more functionalities such as metrology with ultrasonic technology, leak detection with audio patterns, communication with low power and long range radio being added to smart meters. These new functionalities allow utilities to deliver new services such as condition-based maintenance and remote monitoring of meters, which lead to efficient management of the network and better customer experience.

LC-sensing solution with TI FemtoFET and CC1350 Sensor Controller Engine

Bidirectional InfraRed PHY communication with a single IR LED

Some EU standards like EN1434-3 for heat meters require optical interface as per EN62056-21, where two separate IR LEDs are used (one for receive and one for transmit direction). TIDA-01212 shows an alternative approach, which uses a single IR LED to implement a bi-directional IrDA PHY link with 9.6 kbps in half-duplex mode. The design approach can  the system reduce cost of any smart (sub-)metering device by replacing the legacy optical IrDA PHY modules with two separate LEDs.

Calibration and metrology accuracy results

This section discusses the procedure used to calibrate the TIDA-010037 design and the results obtained with this design.

Calibration and metrology accuracy results

This section discusses the procedure used to calibrate the TIDA-010037 design and the results obtained with this design.

Comparisons between isolated shunt sensing architectures

Both isolated modulator and isolated metrology AFE architectures have their advantages with respect to each other.  Depending on system requirements, one architecture may be more feasible than the other.  This section compares the two isolated shunt sensing architectures and discusses which architecture is best for different system requirements.

Current sensor and metrology architecture options

This section compares two types of current sensors used in electricity meters: current transformers and shunts.  In addition, it discusses three different architectures for sensing the voltage and current samples used to calculate the metrology parameters.  These architectures include a SoC-based architecture, AFE-based architecture, and ADC-based architecture.

Current sensor and metrology architecture options

This section compares two types of current sensors used in electricity meters: current transformers and shunts.  In addition, it discusses three different architectures for sensing the voltage and current samples used to calculate the metrology parameters.  These architectures include a SoC-based architecture, AFE-based architecture, and ADC-based architecture.

Decoding PRU-ICSS (hardware and software) for data acquisition

This video dives deeper into the details of the Programmable Real-Time Unit and Industrial Communications Subsystem (PRU-ICSS). The programmable nature of the PRU-ICSS, along with its access to pins, events and all system-on-chip (SoC) resources, provides flexibility in implementing fast, real-time responses, custom peripheral interfaces and the ability to offload tasks from the other processor cores of the SoC. The video also includes a comparison of PRU between different processors.

Design Details for TI design TIDA-00834 High Accuracy Analog Front End Using 16-Bit SAR ADC with ±10V Measurement Range Reference Design

Fifth part of the session will focus on providing detailed information on TIDA-00834 TI design.  The initial slides cover Design Overview, Features, Key Components, test Setup, market differentiators, Block Diagram with links to relevant TI Designs, EVMs and TI product used in this design. Circuit representation and detailed description for ADC interface, Voltage and Current measurement and Power supply are provided. Graphs for Voltage and Current measurement accuracy are shown; along with collaterals and TI design links that can be referred by customers during design.

Designing software for 1-phase electricity meters that use standalone ADCs

This section covers the initialization code and algorithms that can be used to calculate metrology parameters in a single phase system using the sensed voltage and current samples.

Designing software for split-phase electricity meters that use standalone ADCs

This section covers the initialization code and algorithms that can be used to calculate metrology parameters in a split-phase system using the sensed voltage and current samples

Detecting case tamper attacks using inductive switches

The first line of defense against tampering by bypassing current, reversing connections, and disconnecting leads is the meter case. Due to this, it is common for utilities to require some form of intrusion detection system to detect when someone opens a case.  In this section, we will cover how to detect someone trying to open the case of a meter.

76 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki