Sort by:

56 Results

6LoWPAN-based Wireless Network Protocols

This section covers system-level deep dive on key wireless network protocols of 6LoWPAN, RPL, and CoAP for smart grid IoT. 

LC-sensing solution with TI FemtoFET and CC1350 Sensor Controller Engine

7-segment LCD control thru SW and GPIOs

This module covers the “Innovative 7-Segment LCD Control Using GPIO Pins and SW” section of the “Single-chip Smart Water meter with Dual-band RF link and InfraRed port” training series.

AC Analog Input Module Architecture (AIM)

The third part of the session provides details on the need to focus on AC analog input module and its use cases in different types of protection relays, Different types of current sensors and the use cases for these sensors including key advantages and dis-advantages. Explains AC analog input module architecture including block diagram showing the critical products and EERD with different subsystems identified showing different approaches for designing an AC AIM.

EV Charging (Pile) Stations Design Considerations

AC and DC Charging (Pile) Station Design Considerations

Gain a deep dive into common design consideration for a Level 1, 2 or 3 EV charging (pile) station and explore the service equipment block diagram for each.

ADS131M04 current detection mode for detecting neutral removal tampering

This section discusses current detection mode, which is a special low-power mode of the ADS131M04 standalone ADC, that can detect the presence of current when someone has tampered with a meter by removing its neutral connection.

Battery and system monitoring for smart meters

Over the last few years, the industry has been moving from mechanical to fully electronic meters. We have seen more and more functionalities such as metrology with ultrasonic technology, leak detection with audio patterns, communication with low power and long range radio being added to smart meters. These new functionalities allow utilities to deliver new services such as condition-based maintenance and remote monitoring of meters, which lead to efficient management of the network and better customer experience.

LC-sensing solution with TI FemtoFET and CC1350 Sensor Controller Engine

Bidirectional InfraRed PHY communication with a single IR LED

Some EU standards like EN1434-3 for heat meters require optical interface as per EN62056-21, where two separate IR LEDs are used (one for receive and one for transmit direction). TIDA-01212 shows an alternative approach, which uses a single IR LED to implement a bi-directional IrDA PHY link with 9.6 kbps in half-duplex mode. The design approach can  the system reduce cost of any smart (sub-)metering device by replacing the legacy optical IrDA PHY modules with two separate LEDs.

Calibration and metrology accuracy results

This section discusses the procedure used to calibrate the TIDA-010037 design and the results obtained with this design.

Calibration and metrology accuracy results

This section discusses the procedure used to calibrate the TIDA-010037 design and the results obtained with this design.

Comparisons between isolated shunt sensing architectures

Both isolated modulator and isolated metrology AFE architectures have their advantages with respect to each other.  Depending on system requirements, one architecture may be more feasible than the other.  This section compares the two isolated shunt sensing architectures and discusses which architecture is best for different system requirements.

Current sensor and metrology architecture options

This section compares two types of current sensors used in electricity meters: current transformers and shunts.  In addition, it discusses three different architectures for sensing the voltage and current samples used to calculate the metrology parameters.  These architectures include a SoC-based architecture, AFE-based architecture, and ADC-based architecture.

Current sensor and metrology architecture options

This section compares two types of current sensors used in electricity meters: current transformers and shunts.  In addition, it discusses three different architectures for sensing the voltage and current samples used to calculate the metrology parameters.  These architectures include a SoC-based architecture, AFE-based architecture, and ADC-based architecture.

Design Details for TI design TIDA-00834 High Accuracy Analog Front End Using 16-Bit SAR ADC with ±10V Measurement Range Reference Design

Fifth part of the session will focus on providing detailed information on TIDA-00834 TI design.  The initial slides cover Design Overview, Features, Key Components, test Setup, market differentiators, Block Diagram with links to relevant TI Designs, EVMs and TI product used in this design. Circuit representation and detailed description for ADC interface, Voltage and Current measurement and Power supply are provided. Graphs for Voltage and Current measurement accuracy are shown; along with collaterals and TI design links that can be referred by customers during design.

Designing software for 1-phase electricity meters that use standalone ADCs

This section covers the initialization code and algorithms that can be used to calculate metrology parameters in a single-phase system using the sensed voltage and current samples.

Designing software for split-phase electricity meters that use standalone ADCs

This section covers the initialization code and algorithms that can be used to calculate metrology parameters in a split-phase system using the sensed voltage and current samples

Detecting magnetic tampering using hall-effect sensors

For anti-tampering, it is common to try to detect the presence of a strong magnet. In this section, we will cover the use of hall sensors for low-power detection of strong magnetic fields in three dimensions.  Details on our magnetic tamper detection reference design, TIDA-00839, will be provided as well as some of the design considerations that were kept in mind when creating this reference design.  

Differential Temperature Measurement sub-system reference design

TIDA-01526 implements a high-precision Differential Temperature Measurement (DTM) subsystem using a 24-bit, low-power, Delta-Sigma ADC. Heat and cold meter DTM subsystems typically use two 2- or 4-wire RTDs such as PT100, PT500 or PT1000 and can achieve measurement accuracy of 20 mK over a water temperature range of 3°C to 180°C. The MSP430FR6047 application MCU converts the resistance value into a temperature reading in TIDA-01526.

Digital temperature sensor replacement of RTD sensors with TMP116

The TMP116 digital precision temperature sensor for the -55 to +125ºC range achieves higher accuracy than the Class AA PT sensor with a 1-point calibration. A small PCB including TI's TPD1E10B06 or TPD1E04U04 protection devices can be sealed into a RTD metal tube and meet the EN 61000-4-2 and -4-4 levels of ESD protection. The 64-bit internal EEPROM inside TMP116 stores user defined calibration data into the digital temperature sensor, simplifying integration with application MCUs, such as MSP430FR6047, FR6989 or CC13xx/26xx wireless MCU families.

Electrical Fundamentals and Need for power systems protection

Welcome to the world of Power Systems. The first part of the session focuses on Introduction to Power Systems, Goal of Power systems protection, fundamentals of Electricity, AC or DC, Importance of electricity, Power system voltage levels and consumers of electricity. Need and Complexities in protection of power system primary Equipment like Generators, Motors, Transformers and Circuit Breakers and finally analysis of what can go wrong on a transmission line.

EV Charging (Pile) Stations Design Considerations

EV Charging (Pile) Station Subsystem Analysis

While an EV charging station (pile) might seem like a straight forward design, there are many challenges to consider when needing to safely control the power delivery. This training module will provide further insights with a subsystem analysis alongside solution examples that help you mitigate commonly overlooked subsystems including public user interfaces, an authentication mechanism and residential communications in EV charging (pile) stations.

56 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki