Hint: separate multiple terms with commas

E.g., 10/19/2019

E.g., 10/19/2019

Hint: separate multiple terms with commas

E.g., 10/19/2019

E.g., 10/19/2019

Sort by:

55 Results

USB

Learn how to design with USB ICs.

TI Precision Labs

TI Precision Labs (TIPL) is the most comprehensive online classroom for analog signal chain designers. From foundational knowledge to advanced concepts, our logical, sequenced and comprehensive teaching approach is both intuitive and practical. The training series, which includes videos and downloadable reference materials, will deepen the technical expertise of experienced engineers and accelerate the development of those early in their career.

Challenges in today’s Body Control Module (BCM) design

This module discusses discrete implementation typically seen inside automotive body control module to monitor external switches. Common implementation methodology is reviewed in this section, and some of the challenges using discrete implementation is discussed in detail.

How MSDI helps solve system-level challenges in BCM design

In this section, the MSDI concept is introduced and how the MSDI helps solve system challenges is discussed in details

Advanced features of the MSDI

This module discusses some of the advanced features offered by the MSDI, and how a system designer can take advantage of these features to improve their system performance.

Using MSDI in the industrial space

This module discusses how the MSDI device can be used in an industrial data acquisition system in details.

Conclusion and More Information

This module concluds this traning session with highlights of the MSDI value propositions, as well as collaterals available to obtain more information about this MSDI device from Texas Instruments.

DS90UB953/954 System Design & Operation: Overview

This introduction video will give the background on FPD-Link III devices, such as the DS90UB953-Q1/ DS90UB954-Q1; the device's role within Advanced Driver Assist Systems (ADAS) in the automotive industry; and explain their broad appeal to engineers of all experience levels. This is fundamental to diving deeper into a 953/954 system, as well as, the links within the system.

DS90UB953/954 System Design & Operation: Typical Customer Issues

This section frames the design and operation video series by showing why it is important to contextualize customer problems in terms of the links between the devices. 

Specifically, this section will discuss: issues with initializing the camera and issues with reading the incorrect serializer ID from the deserializer.

DS90UB953/954 System Design & Operation: Basic Design Rules

Understanding what hardware and software settings are important is critical to establishing a foundation for the 953/954 system. These settings can occur during or after power up and may need to be changed via software. As a result, these settings are routinely checked and verified before checking any of the other links in the system.

Specifically, this sections discusses: Diagnostics post power up, Mode and IDX Pins, Clocking Modes between the 953/954, Aliasing, I2C Pass Through, Port selection on 954, Analog Launch Pad (ALP), and Successful I2C Communication

DS90UB953/954 System Design & Operation: 953-954 Link Design

This section analyzes the link between the 953 and 954 and establishes how to identify the health and operation of the link. Since the link between the 953-954 is the most fundamental link used to communicate between devices, it is often checked first.

Specifically, this section discusses: Back Channel configuration, Built in Self Test (BIST), Adaptive Equalization (AEQ), and Channel Monitor Loop (CMLOUT)

DS90UB953/954 System Design & Operation: Sensor-953 Link Design

This is the Sensor and 953 Link Design section in DS90UB953/954 System Design & Operation video series. This video discusses how to use the sensor-953 link, as well as, the specific settings that are used with this link.

DS90UB953/954 System Design & Operation: 954-ISP/SoC Link Design

This section discusses what frame synchronization (FrameSync) is and how to configure in on the 953 and 954 and how CSI2 data is transferred across the link from the 954 to the ISP/SoC

Specifically, this section discusses: Frame Synchronization (FrameSync), Controlling 953 GPIOs locally and remotely via I2C, Unsynchronized and synchronized sensors, Internal and External Frame Sync, Port Forwarding, Accessing Indirect Registers, and Pattern Generation on 953 & 954

DS90UB953/954 System Design & Operation: Hardware Design

This section discusses how design a 953/954 using Power over Coax (PoC), and various hardware checks and concepts that need to be considered when analyzing a 953/954 system.

Specifically, this section discusses: Power Over Coax (PoC), AC Coupling Capacitors, PoC Inductors, Typical PoC Schematic, Critical Signal Routing, I2C Pullups, Loop Filter Capacitors on 953, Insertion Loss, Return Loss, and Time Domain Reflection (TDR) measurements.

55 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki