Sort by:

185 Results

MSP430FR5969 LaunchPad Development Kit training series

This six part training walks through the usage of the MSP430FR5969 LaunchPad. The training explains the working of the demo code that is pre-programmed in the LaunchPad. You will also learn how to setup CCS projects and initialize and use key peripherals in the MSP430FR59xx family of MCUs.

MSP430FR4x/FR2x MCU Overview Workshop

The MSP430 ultra-low-power microcontroller family now includes the MSP430FR4x/FR2x series of MCUs with unmatched flexibility in the form of the industry’s lowest-power software-configurable LCD driver, abundant IO and unified non-volatile FRAM. These easy-to-use microcontroller series can be evaluated with the low cost MCU development tool, the MSP430FR4133 LaunchPad. Target Socket boards can also be paired with the MSP-FET programmer/debugger for development in a full system.

Getting started with the MSP430 5xx Experimenters Board (7-part series)

This 7 Part Series with the MSP430 5xx Experimenters Board will cover the following topics:

  • Introduction
  • Active and low power mode operation
  • Mixed signal application example
  • Hardware timers to conserve power
  • Implementing a fully optimized ADC12 routine
  • MSP430 tools, resources, and conclusions

SimpleLink™ MSP432™ low-power + high-performance MCUs training series

While the market requires better power performance, it also continuously demands more functionality from devices. The challenge many developers face today is maintaining or improving battery operating life while simultaneously increasing a device’s capabilities. For many devices, it is not feasible to increase battery size or capacity; this means that developers need to achieve higher performance within the same power footprint, if battery life is not to be compromised.

Teaching Old Motors New Tricks with C2000

While motor topologies have remained relatively unchanged over the past century, control techniques by comparison have experienced explosive growth. This has been driven in large part by technology advancements in the semiconductor industry. This seminar focuses specifically on advancements in the control of motors with an emphasis on field-oriented principles with brushless AC motors.

Control Theory seminar

This 4-part technical seminar offers an introduction to control theory which is of value to electronic, electrical and mechanical engineers.  The aim is to provide engineers with an insight into elementary control problems and their solution.  An understanding of basic engineering mathematics is recommended to benefit fully from this course. 

Agenda
  1. Fundamental concepts: Linear systems, transient response, frequency analysis, classification of systems
  2. Feedback systems: Effects of feedback, Nyquist analysis, stability margins, phase compensation
  3. Transient response: Transient specifications, steady state error, PID control, root locus analysis
  4. Discrete time systems: Sampled systems, the z-transform, aliasing, delay & reconstruction, discrete transformations
Description
  • The course opens with a review of fundamental concepts, including linear differential equations and the Laplace transform. The behaviour of classical first and second order systems is examined in both the time and the frequency domains. 
  • The second section introduces closed loop control and the effects of negative feedback in the frequency domain. The Nyquist plot is introduced as a valuable tool to assess control loop stability and performance, and is applied to the design of phase compensators. 
  • The central theme of section three is control performance in the time domain. The design and tuning of PID controllers is explained using the step response, and various methods of assessing quality of response are presented. The root locus plot then is introduced as a method of designing complex systems to meet transient response specifications. 
  • Section four focuses on discrete time systems.  The z-transform is introduced, and the relationship between the s-plane and z-plane explained in detail.  The design of digital closed loop controllers is then described using emulation and direct design methods.  Also covered are some important practical considerations when implementing discrete time controllers, including aliasing, sample rate selection, the effects of computational delay, and zero order hold.
  • The material is supported by many examples and tutorials, and includes a short question & answer session at the end of each section.  Matlab is used throughout the seminar to introduce new concepts and to illustrate each major topic.  A printed copy of the seminar manual containing the presentation material is issued to each attendee at the start of the course.

C2000 InstaSPIN-FOC Motor Control LaunchPad and BoosterPack

This 6-part series provides information for C2000 InstaSPIN-FOC Motor Control LaunchPad and BoosterPack.

The InstaSPIN™-FOC enabled C2000™ Piccolo LaunchPad is an inexpensive evaluation platform designed to help you leap right into the world of sensorless motor control using the InstaSPIN-FOC solution.

C2000 Concerto F28M3x Microcontroller Training Series

This presentation series will define the position of the Concerto MCU devices in the C2000  MCU family and discuss the features and benefits that make this a no compromise solution. There will be a review of the safety features which have been made necessary by the advances in greener technologies. The intuitive software, which helps reduce time to market will be highlighted and there will be a short discussion of available training and tools

Use MSP432 microcontrollers to bring high performance to low-power applications

While the market requires better power performance, it also continuously demands more functionality from devices. The challenge many developers face today is maintaining or improving battery operating life while simultaneously increasing a device’s capabilities. For many devices, it is not feasible to increase battery size or capacity. Developers need to achieve higher performance within the same power footprint if battery life is not to be compromised.

State Space Control seminar

A 4-part course in control theory based on the spate space modelling paradigm.  This course is often taught in conjunction with the

C2000 InstaSPIN: From evaluation to production

InstaSPIN-FOC is a sensorless field-oriented motor control algorithm which runs on select C2000 devices.  This video series is intended for customers who are currently using or considering InstaSPIN-FOC.  The 7-part series covers four categories of training: Introduction, evaluation, usage (software and hardware), and debugging of InstaSPIN.

MSP430 Capacitive Touch MCUs featuring CapTIvate™ Technology Training Series

MSP430 MCUs featuring CapTIvate technology are the most noise-immune capacitive touch MCUs, and first to feature an IEC61000-4-6 certified solution. These MCUs feature the most configurable combination of buttons, wheels, sliders and proximity sensing interfaces, as well as support for metal touch, glove-proof and moisture-tolerant designs, all at the world's lowest power.

This training series details the key features of MSP430 MCUs featuring CapTIvate technology, enabling you to get started on your next great capacitive touch design and get to market more quickly.

IoT Secure Connection Training Series

Secure Connection to IoT Cloud Server Training Series

As more and more IoT products are being connected to the internet, the security of these devices is becoming increasingly important. A security-focused approach should be taken when building IoT products to protect users’ privacy and block any malicious activity.

Functional safety 4-part training series

Functional safety

Compliance to Functional Safety standards is becoming a requirement for automotive, transportation, medical and many industrial end equipments. Hercules™ MCUs  are based o

Webinar Series

Join our webinar series, as we explore different industry trends and technologies across our diverse product portfolio. Over the coming months, our experts will cover the latest analog, power management and embedded processing topics, across both automotive and industrial applications.

Tech Days

Technical Seminar

Were you unable to attend Tech Day but want to view the featured content? Did you attend and want to revisit a particular session? This series contains many of the sessions from the embedded processing, power supply design, signal chain, and wireless connectivity tracks. In addition, this series features recordings of select TI demos from the exhibitors hall.

Advanced Signal Processing on 16-bit MSP430 FRAM MCUs with Low Energy Accelerator (LEA)

This training series covers LEA or Low Energy Accelerator a vector math co-processor, the performance benchmark, and how to get started on the new MSP430FR599x. LEA is capable of performing various signal processing tasks efficiently without any CPU intervention. For example, LEA can perform a 256-point complex FFT in just ~5k cycles whereas a Cortex-M4F would take approximately 17k cycles (3.6x improvement).

Embedded Security Fundamentals and Portfolio Overview for MSP MCUs Series

This series outlines a number of Embedded Security Fundamentals as well as a portfolio overview for MSP430 and MSP432 microcontrollers. These are just some of the topics covered in this series:

  • Understand embedded security fundamentals
  • Security terminologies and definitions 
  • Embedded microcontroller user requirements
  • Microcontroller devices security offerings and development model
High efficiency power and motor drive systems with C2000, GaN and INA240 current sensing

Designing for high-efficiency power and motor drive applications

Learn about solutions that pair the flexibility of digital power control with C2000 MCUs and in-line current sensing with the high-power efficiency of GaN. 

SimpleLink Academy for Sub-1 GHz

SimpleLink™ Academy for Sub-1 GHz CC13x0 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink CC13x0 Wireless MCUs.

185 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki