Sort by:

69 Results

MSP-EXP430FR5969 - 6 Part Series

This six part training walks through the usage of the MSP430FR5969 LaunchPad. The training explains the working of the demo code that is pre-programmed in the LaunchPad. You will also learn how to setup CCS projects and initialize and use key peripherals in the MSP430FR59xx family of MCUs.

 

MSP430FR4x/FR2x MCU Overview Workshop

The MSP430 ultra-low-power microcontroller family now includes the MSP430FR4x/FR2x series of MCUs with unmatched flexibility in the form of the industry’s lowest-power software-configurable LCD driver, abundant IO and unified non-volatile FRAM. These easy to use microcontroller series can be evaluated with the low cost MCU development tool, the MSP430FR4133 LaunchPad. Target Socket boards can also be paired with the MSP-FET programmer/debugger for development in a full system.

MSP432™ Low-Power + High Performance MCUs Training Series

While the market requires better power performance, it also continuously demands more functionality from devices. The challenge many developers face today is maintaining or improving battery operating life while simultaneously increasing a device’s capabilities. For many devices, it is not feasible to increase battery size or capacity; this means that developers need to achieve higher performance within the same power footprint, if battery life is not to be compromised.

Control Theory Seminar - 4 Part Series

This technical seminar offers an introduction to control theory which will be valuable to electronic, electrical and mechanical engineers.  The aim is to provide engineers with an insight into elementary control problems and their solution.  An understanding of basic engineering mathematics is recommended to benefit fully from this course. 

C2000 InstaSPIN-FOC Motor Control LaunchPad and BoosterPack - 6 Part Series

This 6 part series provides information for C2000 InstaSPIN-FOC Motor Control LaunchPad and BoosterPack.

The InstaSPIN™-FOC enabled C2000™ Piccolo LaunchPad is an inexpensive evaluation platform designed to help you leap right into the world of sensorless motor control using the InstaSPIN-FOC solution.

C2000 CLA C Compiler - 4 Part Series

This online training series will teach you the details necessary to utilize the Control Law Accelerator (CLA)

TM4C129x MCUs Series

This 6-part training will provide technical overviews of various features on the TM4C129x Series Microcontrollers developed specifically for applications that simultaneously connect, communicate and control.

C2000 Concerto F28M3x Microcontroller Training Series

This presentation series will define the position of the Concerto MCU series in the C2000  MCU family and discuss the features and benefits that make this a no compromise solution. There will be a review of the safety features which have been made necessary by the advances in greener technologies. The intuitive software, which helps reduce time to market will be highlighted and there will be a short discussion of available training and tools

Use MSP432 Microcontrollers to Bring High Performance to Low-Power Applications

While the market requires better power performance, it also continuously demands more functionality from devices. The challenge many developers face today is maintaining or improving battery operating life while simultaneously increasing a device’s capabilities. For many devices, it is not feasible to increase battery size or capacity.

State Space Control Seminar - 4 Part Series

A 1-day course in control theory based on the spate space modelling paradigm.  This course is often taught in conjunction with the

MSP430 Capacitive Touch MCUs featuring CapTIvate™ Technology Training Series

MSP430 MCUs featuring CapTIvate technology are the most noise-immune capacitive touch MCUs, and first to feature an IEC61000-4-6 certified solution. These MCUs feature the most configurable combination of buttons, wheels, sliders and proximity sensing interfaces, as well as support for metal touch, glove-proof and moisture-tolerant designs, all at the world's lowest power.

This training series details the key features of MSP430 MCUs featuring CapTIvate technology, enabling you to get started on your next great capacitive touch design and get to market more quickly.

MSP MCU Crypto-Bootloader Training Series

In-field firmware updates are becoming an increasingly popular feature supported on products that are deployed to the field; however, this feature is also very commonly exploited by attackers, and if vulnerable, can compromise the security of the system. In this series we will discuss the various  security concerns for in-field firmware updates, and a solution for increasing the security of in-field firmware updates in ultra-low power MSP microcontrollers - called the Crypto-Bootloader. 

IoT Secure Connection Training Series

Secure Connection to IoT Cloud Server Training Series

As more and more IoT products are being connected to the internet, the security of these devices is becoming increasingly important. A security-focused approach should be taken when building IoT products to protect users’ privacy and block any malicious activity.

Advanced Signal Processing on 16-bit MSP430 FRAM MCUs with Low Energy Accelerator (LEA)

This training series covers LEA or Low Energy Accelerator a vector math co-processor, the performance benchmark, and how to get started on the new MSP430FR599x. LEA is capable of performing various signal processing tasks efficiently without any CPU intervention. For example, LEA can perform a 256-point complex FFT in just ~5k cycles whereas a Cortex-M4F would take approximately 17k cycles (3.6x improvement).

Embedded Security Fundamentals and Portfolio Overview for MSP MCUs Series

This series outlines a number of Embedded Security Fundamentals as well as a portfolio overview for MSP430 and MSP432 microcontrollers. These are just some of the topics covered in this series:

  • Understand embedded security fundamentals
  • Security terminologies and definitions 
  • Embedded microcontroller user requirements
  • Microcontroller devices security offerings and development model
High efficiency power and motor drive systems with C2000, GaN and INA240 current sensing

Designing for high-efficiency power and motor drive applications

Learn about solutions that pair the flexibility of digital power control with C2000 MCUs and in-line current sensing with the high-power efficiency of GaN. 

SimpleLink Academy for Sub-1 GHz

SimpleLink™ Academy for Sub-1 GHz CC13x0 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink CC13x0 Wireless MCUs.

SimpleLink Academy for MSP432

SimpleLink™ Academy for MSP432 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink MSP432 Host MCU.

SimpleLink Academy for Wi-Fi

SimpleLink™ Academy for Wi-Fi® CC3x20 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink CC32x0 Wireless MCU.

SimpleLink Academy - Bluetooth low energy

SimpleLink™ Academy for Bluetooth® low energy CC2640R2 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink CC2640R2 Wireless MCU.

69 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki