Sort by:

38 Results

MSP-EXP430FR5969 - 6 Part Series

This six part training walks through the usage of the MSP430FR5969 LaunchPad. The training explains the working of the demo code that is pre-programmed in the LaunchPad. You will also learn how to setup CCS projects and initialize and use key peripherals in the MSP430FR59xx family of MCUs.

Getting Started with the MSP430 5xx Experimenters Board - 7 Part Series

This 7 Part Series with the MSP430 5xx Experimenters Board will cover the following topics:

  • Introduction
  • Active and low power mode operation
  • Mixed signal application example
  • Hardware timers to conserve power
  • Implementing a fully optimized ADC12 routine
  • MSP430 tools, resources, and conclusions

MSP430 Capacitive Touch MCUs featuring CapTIvate™ Technology Training Series

MSP430 MCUs featuring CapTIvate technology are the most noise-immune capacitive touch MCUs, and first to feature an IEC61000-4-6 certified solution. These MCUs feature the most configurable combination of buttons, wheels, sliders and proximity sensing interfaces, as well as support for metal touch, glove-proof and moisture-tolerant designs, all at the world's lowest power.

This training series details the key features of MSP430 MCUs featuring CapTIvate technology, enabling you to get started on your next great capacitive touch design and get to market more quickly.

Advanced Signal Processing on 16-bit MSP430 FRAM MCUs with Low Energy Accelerator (LEA)

This training series covers LEA or Low Energy Accelerator a vector math co-processor, the performance benchmark, and how to get started on the new MSP430FR599x. LEA is capable of performing various signal processing tasks efficiently without any CPU intervention. For example, LEA can perform a 256-point complex FFT in just ~5k cycles whereas a Cortex-M4F would take approximately 17k cycles (3.6x improvement).

Anti-tamper Techniques to Thwart Attacks on Smart Meters

Non-technical losses (“theft”) account for billions of dollars of revenue loss for utility providers around the world as individuals are able to hack meters to slow or stop the accumulation of energy usage statistics. This loss has driven increased requirements for enhancing the protection designed into new smart meters.  This training session will discuss different methods of attacking smart meters and how TI’s analog portfolio can be used to detect or even prevent these attacks. In one scenario magnets are used to saturate any transformers present in the system.

Designing with Delta-Sigma ADCs: System design considerations to optimize performance

Delta-sigma analog-to-digital converters (ADCs) are oversampling converters typically used in applications requiring higher resolution. However, ADCs do not work by themselves. In fact, they require several key components around them, including a front-end amplifier, a voltage reference, a clock source, power supplies, and a good layout. Many devices integrate these features together with the ADC to offer a complete system solution, which simplifies the design for customers and minimizes board space.

Ultrasonic water meters have improved accuracy and precision to detect the smallest leaks to reduce water waste.

Ultrasonic Sensing for More Accurate and Precise Water Flow Meters

Ultrasonic sensing techniques have been popular in smart water meters because the technology avoids any moving parts which are prone to degrade over the lifetime of the product. The MSP430FR6047 microcontroller (MCU) family takes ultrasonic sensing solutions to next level of performance delivering <25ps of accuracy, detection of low flow rates <1 liter/hour and high precision of <5ps.

MSP-EXP430FR2433 – the MSP430FR2433 Microcontroller LaunchPad Development Kit

MSP-EXP430FR2433 LaunchPad Development Kit Training

The MSP-EXP430FR2433 LaunchPad™ development kit is a member of the MSP430™ Value Line Sensing MCU family. The LaunchPad kit provides a quick evaluation and prototyping tool for the MSP430FR2433 microcontroller (MCU). This series provides an overview of the LaunchPad kit’s features and the out-of-box temperature sensing demo.

25 functions for 25 cents using TI’s MSP430 Value Line Sensing microcontrollers

25 Functions for 25 Cents Video Series

Simple functions such as timer replacement, input/output expanders, system reset controllers and stand-alone EEPROM are common on PCBs. Low-cost, ultra-low-power MSP430™ value line  microcontrollers (MCUs) offer cost savings when replacing digital and analog functions in a system. Watch this series to see how MSP430 MCUs can be used to enhance communication, pulse width modulation, systems and housekeeping, and timer functions in your next design.

MSP430 Training Series

MSP430 Workshop Series

This workshop is designed to help users gain an in-depth knowledge about the MSP430 family of microcontrollers.

Getting Started MSP430G2553 Value Line LaunchPad Workshop Series

This series will walk you through the MSP430G2553 Value-Line Microcontroller LaunchPad and its peripherals.

Precision temperature measurement in heat and cold meters

PT100/500/1000 Resistance Temperature Detectors (RTDs) are widely used in grid infrastructure and factory automation applications where high precision temperature measurement is often required. Technical requirements include either 20 mK precise Differential Temperature Measurement (DTM) for heat and cold meters from 0 to 180°C or better than 400 mK precision over the full range of -200 to 850°C for industrial sensor transmitters.

The MSP-EXP430FR2355 LaunchPad development kit training

MSP-EXP430FR2355 LaunchPad Development Kit Training

The MSP-EXP430FR2355 LaunchPad™ development kit is a member of the MSP430™ Value Line MCU family. The LaunchPad kit provides a quick evaluation and prototyping tool for the MSP430FR2355 microcontroller (MCU). This series provides an overview of the LaunchPad kit’s features and the out-of-box light sensing and smart analog combo GUI demos.

Ultrasonic sensing gas flow metering video series

This video series provides an overview of our ultrasonic sensing solutions for gas flow metering using the MSP430FR6043 family of system-on-chips including the EVM (EVM430-FR6043) as well as the design GUI and software through the ultrasonic design center. 

Why design with MSP430FR2355?

The MSP430FR2355 is designed to match your project needs, by adding more analog features, extending the temperature range and extending a broad MSP430 MCU portfolio.  This 4-part series showcases the MSP430FR2355 device and how it can help you solve your design challenges.

TI-RTOS Workshop Series

This workshop will support the following products - Tiva-C series, MSP430, C6000 and C28x. If you are an AM335x (ARM Cortex A8) user, almost 100% of what is covered in the workshop applies to this target as well with the exception of interrupts and timers. TI-RTOS is mostly target agnostic, so ANY user of ANY TI platform that supports TI-RTOS will learn a ton about the kernel (SYS/BIOS). Also, any Keystone (C66x) users will be able to learn SYS/BIOS in this workshop using the C6748 LCDK platform.

Capacitive Touch Basics with MSP430 MCUs featuring CapTIvate Technology

This section of the video series provides an introduction to capacitive touch using MSP430 MCUs with CapTIvate technology as well as how to get started with CapTIvate Design Center and CapTIvate development tools.

Fundamental PCB Layout and Design Guidelines of MSP430 MCUs with CapTIvate Technology

This training covers the fundamental design techniques required to implement a successful capacitive sensing hardware design. This series will explore a number of design topics, including:  Basic layout guidelines overlays, back lighting; Dealing with moisture; Self capacitance sensors; Mutual capacitance sensors; and Proximity sensors.

Introduction to EMC Challenges and Design with CapTIvate MCUs

This video series provides a reference on designing capacitive touch capabilities to withstand EMC challenges commonly found in human machine interface applications.

Application Demos of Capacitive Touch Featuring MSP430 MCUs with CapTIvate Technology

Capacitive sensing enables buttons, sliders, wheels and proximity features to be added to a wide-range of applications including building and home access panels and security systems, appliances, personal electronics and more. Watch the videos in this series to get an idea of the capabilities CapTIvate technology can bring to your next application.
38 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki