Sort by:

58 Results

MSP432™ Low-Power + High Performance MCUs Training Series

While the market requires better power performance, it also continuously demands more functionality from devices. The challenge many developers face today is maintaining or improving battery operating life while simultaneously increasing a device’s capabilities. For many devices, it is not feasible to increase battery size or capacity; this means that developers need to achieve higher performance within the same power footprint, if battery life is not to be compromised.

Use MSP432 Microcontrollers to Bring High Performance to Low-Power Applications

While the market requires better power performance, it also continuously demands more functionality from devices. The challenge many developers face today is maintaining or improving battery operating life while simultaneously increasing a device’s capabilities. For many devices, it is not feasible to increase battery size or capacity.

Embedded Security Fundamentals and Portfolio Overview for MSP MCUs Series

This series outlines a number of Embedded Security Fundamentals as well as a portfolio overview for MSP430 and MSP432 microcontrollers. These are just some of the topics covered in this series:

  • Understand embedded security fundamentals
  • Security terminologies and definitions 
  • Embedded microcontroller user requirements
  • Microcontroller devices security offerings and development model
SimpleLink Academy for Sub-1 GHz

SimpleLink™ Academy for Sub-1 GHz CC13x0 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink CC13x0 Wireless MCUs.

SimpleLink Academy for MSP432

SimpleLink™ Academy for MSP432 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink MSP432 Host MCU.

SimpleLink Academy - Bluetooth low energy

SimpleLink™ Academy for Bluetooth® low energy CC2640R2 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink CC2640R2 Wireless MCU.

SimpleLink Academy for Wi-Fi

SimpleLink™ Academy for Wi-Fi® CC3x20 SDK

Below are the SimpleLink Academy modules associated to the SimpleLink CC32x0 Wireless MCU.

Introduction to SimpleLink SDK

Introduction to the SimpleLink SDK

Provides details of the software, hardware, tools, and resource components that make up the SimpleLink SDK software development kit, with an overview of TI-RTOS concepts and labs illustrating how to use the SDK to build and port applications between SimpleLink devices.

Bluetooth 5 Overview on the SimpleLink CC2640R2F wireless MCU

Introducing TI's fully qualified hardware and software solution for Bluetooth 5.

iOS/Android-Based Firmware Updates for SimpleLink Devices Training Series

This training series consists of everything a user needs to get started with updating the firmware running on their SimpleLink MSP432 device over BLE with a focus on the host side iOS and Android development. Technical details involving various components of mobile application development using BLE are covered copiously and reference applications for both iOS and Android are provided to users to use as a template for their designs.

MSP Crypto Bootloader Training Series

In-field firmware updates are becoming an increasingly popular feature supported on products that are deployed to the field; however, this feature is also very commonly exploited by attackers, and if vulnerable, can compromise the security of the system.

SimpleLink Academy for Sub-1 GHz

POSIX

The SimpleLink™ SDK features POSIX (Portable Operating System Interface), which is a family of standards specified by the IEEE Computer Society for maintaining compatibility between operating systems. Through POSIX-compliant APIs, developers can maintain 100% application code portability between various OS/kernels.

SimpleLink Academy for Sub-1 GHz

Proprietary RF

The CC13x0 wireless MCU features an integrated radio, which can be programmed to support various protocols. The CC1310 device features a sub-GHz RF radio, while the CC1350 device features a dual-band radio capable of both sub-GHz and 2.4GHz.

58 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki