Hint: separate multiple terms with commas

E.g., 09/19/2019

E.g., 09/19/2019

Hint: separate multiple terms with commas

E.g., 09/19/2019

E.g., 09/19/2019

Sort by:

59 Results
2016 工業應用技術專題

2016 工業應用技術專題

在訊號鏈單元,教您如何判斷、解決運算放大器震盪問題,並運用 TI Design 加速、瞭解設計流程,以及隔離設計在惡劣的工業環境中,面臨提高訊號的穩健性和可靠度的挑戰該如何應對。電源管理單元則帶您了解 PoE的基本概念,探討電源系統及隔離型交換式電源供應器的基礎和原理,如功率因素調整、返馳式、順向式、半橋諧振式及全橋式。此外,本次線上培訓也加入嵌入式處理器以及 DLP 等主題分享。  

25 functions for 25 cents using TI’s MSP430 Value Line Sensing microcontrollers

25 Functions for 25 Cents Video Series

Simple functions such as timer replacement, input/output expanders, system reset controllers and stand-alone EEPROM are common on PCBs. Low-cost, ultra-low-power MSP430™ value line  microcontrollers (MCUs) offer cost savings when replacing digital and analog functions in a system. Watch this series to see how MSP430 MCUs can be used to enhance communication, pulse width modulation, systems and housekeeping, and timer functions in your next design.

66AK2Gx Processor Training Series

Similar to existing KeyStone-based SoC devices, the 66AK2Gx enables both the DSP and ARM cores to master all memory and peripherals in the system. This architecture facilitates maximum software flexibility where either DSP- or ARM-centric system designs can be achieved. 

This curriculum provides an in-depth look at the K2G Processors, Processor SDK-Linux and TI-RTOS, and the Programmable Realtime Unit (PRU).

AM6x Sitara™ Processors Training Series

TI’s AM6x Sitara processor family, along with the Processor SDK, brings unparalleled scalability, reliability, integration, and ease-of-use to the Sitara product line. The new, highly-integrated Sitara AM6x processor family provides industrial-grade reliability, with quad and dual Arm® Cortex®-A53 core variants built to meet the rapidly evolving needs of Industry 4.0 in factory automation and grid infrastructure.

Anti-tamper Techniques to Thwart Attacks on Smart Meters

Non-technical losses (“theft”) account for billions of dollars of revenue loss for utility providers around the world as individuals are able to hack meters to slow or stop the accumulation of energy usage statistics. This loss has driven increased requirements for enhancing the protection designed into new smart meters.  This training session will discuss different methods of attacking smart meters and how TI’s analog portfolio can be used to detect or even prevent these attacks. In one scenario magnets are used to saturate any transformers present in the system.

Battery and system monitoring for smart meters

Over the last few years, the industry has been moving from mechanical to fully electronic meters. We have seen more and more functionalities such as metrology with ultrasonic technology, leak detection with audio patterns, communication with low power and long range radio being added to smart meters. These new functionalities allow utilities to deliver new services such as condition-based maintenance and remote monitoring of meters, which lead to efficient management of the network and better customer experience.

Battery Powered Motor Drives: How to Design a High Performance Power Stage?

Modern battery powered motor drive applications such as power tools, drones, vacuum cleaners, eBikes, etc. show a clear trend towards permanent magnet synchronous motors (PMSM) and brushless DC motors (BLDC). The biggest challenge in designing the power stage for these applications is to meet form factor, efficiency, protection, peak current carrying capability and thermal performance. This training will explain how to do a system design to meet the design challenges  by proper selection of power FET and gate driver.

Solution for industrial drives and motor control

C2000 DesignDRIVE: Solution for industrial drives and motor control

This training is meant for engineers designing the control circuits for servo or AC inverter motor controllers for industrial machinery. In particular, the on-demand curriculum is for those who are planning to develop their next drive system based on a C2000™ microcontroller (MCU) and are interested in quickly learning how to use the DesignDRIVE solutions available from TI.

C55x Digital Signal Processors Training Series

TI’s TMS320C55x Fixed-Point Digital Signal Processors (DSP) enable high performance and low power through increased parallelism and total focus on power savings. Industry-leading active power enables computationally-intensive applications, such as voice triggering and encoding, to run on battery for extended period of time. Development tools include the award-winning eXpressDSP, Code Composer Studio (CCS), Integrated Development Environment (IDE), DSP/BIOS, optimized DSP and math libraries, and the industry’s largest third-party network.

Create an Industrial 3D Machine Vision System using DLP® Technology

Create an Industrial 3D Machine Vision System using DLP® Technology

This DLP® training series helps users understand the most common 3D machine vision techniques.  The series includes the following key content:

Customizing a Yocto-Based Linux Distribution for Production: Training Series

Every customer going to production with a Linux-based system wants a filesystem that is tailored to their system.  The filesystem provided with the Processor SDK is a great starting point that contains many popular applications and utilities.

Debugging Embedded Linux Systems Training Series

Linux is well-adopted within embedded systems. But debugging Linux system issues can be overwhelming. This training series teaches the techniques of debugging kernel issues that may be encountered in embedded Linux systems. This training series explains the Linux kernel logging system and logging API, illustrates how to locate a particular device driver, and demonstrates how to read kernel oops logs.

Designing 6.6kW Bidirectional HEV/EV On-Board-Charger with SiC and Embedded Technologies

In this series of presentations, we go through the HEV/EV market status and history, OBC specifications, technology trend, topology selections and design considerations of an OBC system. Complete test results of a 6.6kW OBC reference design (Including AC-DC rectifier and isolated DC-DC converter) will be shown in the end of this paper to demonstrate the performance of our TIDesigns as well as TI SiC and embedded Technologies.

Embedded Security Fundamentals and Portfolio Overview for MSP MCUs Series

This series outlines a number of Embedded Security Fundamentals as well as a portfolio overview for MSP430 and MSP432 microcontrollers. These are just some of the topics covered in this series:

  • Understand embedded security fundamentals
  • Security terminologies and definitions 
  • Embedded microcontroller user requirements
  • Microcontroller devices security offerings and development model

Energy Measurement Design Center for MSP430 MCUs: Training Series

This training series provides information on the Energy Measurement Design Center for MSP430 MCUs.

EtherCAT® Master on Sitara™ Processors Training Series

This training presents TI’s ready-to-use EtherCAT masters solutions for Sitara processors. EtherCAT master on Sitara runs on different operating systems, including TI-RTOS and RT Linux. It also runs on the EMAC interfaces (CPSW and PRU ICSS_EMAC) of any Sitara device, including AM57x, AM437x, and AM335x.

From Zero to Hero: Time-of-Flight Training (ToF) Series

From Zero to Hero: Time-of-Flight (ToF) Training Series

This training series will teach you about time-of-flight (ToF) technology and provide some tools and resources to help you prototype faster.

Getting started with the AFE74xx RF-sampling transceiver

Quickly evaluate the AFE7444 and/or AFE7422 RF-sampling transceiver with this series of how to videos.

How to design 1-phase shunt electricity meters using standalone metrology ADCs

As processing requirements for electricity meters gradually increase, it becomes increasingly difficult to find one device that meets both the processing requirements for adding advanced metrology features to smart meters while also accurately sensing metrology parameters, such as RMS voltage, RMS current and active power.  To deal with this design challenge, one option is to use a separate metrology microcontroller and a standalone ADC.

How to design high-accuracy CT-based split-phase electricity meters using standalone metrology ADCs

As processing requirements for electricity meters gradually increase, it becomes increasingly difficult to find one device that meets both the processing requirements for adding advanced metrology features to smart meters while also accurately sensing metrology parameters, such as RMS voltage, RMS current, and active power.  To deal with this design challenge, one option is to use a separate metrology microcontroller and a standalone ADC.

59 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki