Sort by:

14 Results
South Asia Industrial Webinar

2018 South Asia Industrial Webinar Series

The topics will cover system design issue and solution for Building Automation, Power Delivery and Test & Measurement. TI experts introduce the latest technology and innovation system reference design. Discover ways to enhance the time-to-market and create safer and efficient industrial systems.

Anti-tamper Techniques to Thwart Attacks on Smart Meters

Non-technical losses (“theft”) account for billions of dollars of revenue loss for utility providers around the world as individuals are able to hack meters to slow or stop the accumulation of energy usage statistics. This loss has driven increased requirements for enhancing the protection designed into new smart meters.  This training session will discuss different methods of attacking smart meters and how TI’s analog portfolio can be used to detect or even prevent these attacks. In one scenario magnets are used to saturate any transformers present in the system.

South Asia Industrial Webinar

Demystifying circuit design with Precision DAC

The presentation addresses the Precision DAC Architecture overview, DAC spec parameters and the theory of operation & Design example. All the information is importer for engineer when work on the system design.

South Asia Industrial Webinar

Design considerations for USB type-C power delivery

The presentation addresses the design consideration of USB Type-C power delivery. USB Type-C is the new trend of Industrial, automotive and personal electronics devices. In the training, audience will be able to learn more about USB Type-C power delivery (PD) requirement and understand architecture of USB Type-C PD, AC/DC power source.

Detecting case tamper attacks using inductive switches

The first line of defense against tampering by bypassing current, reversing connections, and disconnecting leads is the meter case. Due to this, it is common for utilities to require some form of intrusion detection system to detect when someone opens a case.  In this section, we will cover how to detect someone trying to open the case of a meter.

Detecting magnetic tampering using hall-effect sensors

For anti-tampering, it is common to try to detect the presence of a strong magnet. In this section, we will cover the use of hall sensors for low-power detection of strong magnetic fields in three dimensions.  Details on our magnetic tamper detection reference design, TIDA-00839, will be provided as well as some of the design considerations that were kept in mind when creating this reference design.  

South Asia Industrial Webinar

Environmental sensor for building automation design

Building automation system is a communication network infrastructure that manages the building service. This training will introduce the environmental sensor black diagram, key reference design and the solution for IC temperature sensor, power saving analog temperature sensor, digital temperature sensor … etc.

Hardening a meter against magnetic tamper attacks

In this section, we will cover how to harden a meter against these magnetic tamper attacks by using shunts for current sensors. For poly-phase implementations, I will go over how to use isolated delta sigma modulators to add the necessary isolation to use shunt current sensors and create magnetically immune poly-phase energy measurement systems. The TIDA-00601 and TIDA-01094 reference designs, which show how to implement a poly-phase isolated shunt measurement system, will be discussed as well as the associated AMC1304 high-side power supplies used in these designs.

How High-Voltage Isolation Technology Works

Want to understand how high-voltage isolation technology works? Watch and learn about reliability testing for isolation. Filmed in TI's high-voltage lab, this series of videos will focus on capacitive isolation structure, working voltage reliability, withstand voltage capability, methods for testing reliability, and more.

South Asia Industrial Webinar

Introduce high power DC/DC conversion design: comparison of PSFB and FB-LLC

The “conventional wisdom” is that the Phase Shifted Full Bridge (PSFB) topology is the best choice for high power DC/DC converter applications. However, the “conventional wisdom” has been challenged by the users who are choosing the Full Bridge LLC (FB-LLC) topology for applications where we would normally suggest the PSFB topology. The speaker provides a clear comparison between the two typologies and tries to indicate which is best in a given application.

Introduction

This section covers what is meter tampering, why is this a problem for utility providers, and some common ways a meter is tampered.

South Asia Industrial Webinar

Overview of commonly-used interface for industrial application

The training provides a very comprehensive introduction of the commonly-used interfaces including RS-485, RS-422, ProfiBus, RS-232, IO-Link, CAN and LIN. These interfaces are used in the application of Factory Automation and some other industrial applications. For the engineer who needs to deal with interface system design, this is a very useful training.

South Asia Industrial Webinar

SAR ADC Design

Targeting the Test and Measurement application, this section includes many topics relevant to designing with SAR ADC devices.

Summary

In this section, a summary of the entire “Anti-tamper Techniques to Thwart Attacks on Smart Meters” training module would be covered.  This summary would cover the “Detecting case tamper attacks using inductive switches “, “Detecting magnetic tampering using hall-effect sensors “,  and “Hardening a meter against magnetic tamper attacks “ sections of the training series. Links will be provided for the reference designs and design tools that were discussed during this training series.

14 Results
arrow-topclosedeletedownloadmenusearchsortingArrowszoom-inzoom-out arrow-downarrow-uparrowCircle-leftarrowCircle-rightblockDiagramcalculatorcalendarchatBubble-doublechatBubble-personchatBubble-singlecheckmark-circlechevron-downchevron-leftchevron-rightchevron-upchipclipboardclose-circlecrossReferencedashdocument-genericdocument-pdfAcrobatdocument-webevaluationModuleglobehistoryClockinfo-circlelistlockmailmyTIonlineDataSheetpersonphonequestion-circlereferenceDesignshoppingCartstartoolsvideoswarningwiki